complexType BudgetExpressionType
diagram plmxml_diagrams/plmxml_p244.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:GeneralExpressionBase
properties
base plm:GeneralExpressionBase
children plm:Description plm:ApplicationRef plm:Attribute
used by
element BudgetExpression
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
expression  xsd:string  required      
format  plm:ExpressionFormatEnum  optional      
annotation
documentation

      An expression for a budget definition.

      Attributes:

      expression:       Inherited from GeneralExpression. Takes values like SUM,
                        MIN, MAX or AVG.
      format:           Inherited from GeneralExpression. Must be set to
                        "excel" in this context.
     
source <xsd:complexType name="BudgetExpressionType">
 
<xsd:annotation>
   
<xsd:documentation>
      An expression for a budget definition.

      Attributes:

      expression:       Inherited from GeneralExpression. Takes values like SUM,
                        MIN, MAX or AVG.
      format:           Inherited from GeneralExpression. Must be set to
                        "excel" in this context.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:GeneralExpressionBase"/>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy