element ConductorOccurrence
diagram plmxml_diagrams/plmxml_p1780.png
namespace http://www.plmxml.org/Schemas/PLMXMLRouteListSchema
type routelist:ConductorOccurrenceType
substitution group routelist:RouteListElement
properties
content complex
children plm:Description plm:ApplicationRef plm:UserData
used by
complexType ConnectionType
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
uniqueId  xsd:normalizedString  required      
documentation
Unique identifier of the RouteList object.
conductorRef  plm:anyURIType  required      
documentation
Reference to Wire, Cable, or Space Reservation element. The resolution is based on the Type.
wireClass  derived by: xsd:NMTOKEN  optional      
wireSignal  xsd:normalizedString  optional      
wireSeparationCode  xsd:normalizedString  optional      
location  xsd:integer  optional      
documentation
Location of the assigned conductor.
        (1. Ordering of the wire in a flat cable
        2. Ordering of the cable in a stacked flat cables.)
length  xsd:double  optional      
documentation
Length of the connection. This is export only field from UG-NX.
cutLength  xsd:double  optional      
documentation

                            Cut length calculated based on the offset and
                            multiplier defined by the assigned conductor (Wire,
                            Cable, Space reservation).  This is export only.
                       
routed  derived by: xsd:NMTOKEN  optional      
documentation
This is export only field
        Auto - Routed automatically
        Manual - Routed Manually
        Not Routed
harnessRef  plm:anyURIType  optional      
documentation
Reference to the Harness to which the wire/cable/space-reservation occurance belongs.
source <xsd:element name="ConductorOccurrence" type="routelist:ConductorOccurrenceType" substitutionGroup="routelist:RouteListElement"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy