complexType ConstraintInstanceType
diagram plmxml_diagrams/plmxml_p843.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:GDEInstanceType
properties
base plm:GDEInstanceType
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Transform plm:Representation plm:VariantCondition plm:Reference plm:PropertyGroup plm:EntityPropertyGroup plm:ConstraintData plm:ConstraintTargetRef plm:JointData plm:FrictionData plm:DriverData plm:ForceData plm:SpringData plm:DamperData plm:BushingData plm:ContactData plm:CouplerData plm:LimitsDependencyData
used by
element ConstraintInstance
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
instancedRef  plm:anyURIType  optional      
transformRef  xsd:IDREF  optional      
materialRef  xsd:IDREF  optional      
partRef  plm:anyURIType  optional      
representationRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
designRequired  xsd:boolean  optional      
quantity  xsd:double  optional      
unitRef  xsd:IDREF  optional      
instanceType  xsd:string  optional      
sequenceNumber  xsd:nonNegativeInteger  optional      
instanceThreadRef  plm:anyURIType  optional      
instanceTypeRef  plm:anyURIType  optional      
instanceNumber  xsd:integer  optional      
annotation
documentation

          This subclass of GDEInstance may be used for instancing a Constraint.

          If a particular type of sub-element is present, the ConstraintInstance
          overrides the entire set of sub-elements of that type present under
          the Constraint.

          Sub-elements:

          ConstraintData: Overrides the data defining the geometric Constraint
                        or the Contact Constraint.
          ConstraintTargetRef: Overrides references to constrained geometry.
          JointData:    Overrides additional data for a Joint Constraint.
          FrictionData: Overrides additional data for a Friction Constraint or a
                        Joint Constraint.
          DriverData:   Overrides additional data for a Driver Constraint or a
                        Joint Constraint.
          ForceData:    Overrides additional data for a Force Constraint.
          SpringData:   Overrides additional data for a Spring Constraint.
          DamperData:   Overrides additional data for a Damper Constraint.
          BushingData:  Overrides additional data for a Bushing Constraint.
          ContactData:  Overrides additional data for a Contact Constraint.
          CouplerData:  Overrides additional data for a Coupler Constraint or a
                        Joint Constraint that infers a Joint.
          LimitsDependencyData: Additional data for a Limits Dependency
                        Constraint.
         
source <xsd:complexType name="ConstraintInstanceType">
 
<xsd:annotation>
   
<xsd:documentation>
          This subclass of GDEInstance may be used for instancing a Constraint.

          If a particular type of sub-element is present, the ConstraintInstance
          overrides the entire set of sub-elements of that type present under
          the Constraint.

          Sub-elements:

          ConstraintData: Overrides the data defining the geometric Constraint
                        or the Contact Constraint.
          ConstraintTargetRef: Overrides references to constrained geometry.
          JointData:    Overrides additional data for a Joint Constraint.
          FrictionData: Overrides additional data for a Friction Constraint or a
                        Joint Constraint.
          DriverData:   Overrides additional data for a Driver Constraint or a
                        Joint Constraint.
          ForceData:    Overrides additional data for a Force Constraint.
          SpringData:   Overrides additional data for a Spring Constraint.
          DamperData:   Overrides additional data for a Damper Constraint.
          BushingData:  Overrides additional data for a Bushing Constraint.
          ContactData:  Overrides additional data for a Contact Constraint.
          CouplerData:  Overrides additional data for a Coupler Constraint or a
                        Joint Constraint that infers a Joint.
          LimitsDependencyData: Additional data for a Limits Dependency
                        Constraint.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:GDEInstanceType">
     
<xsd:sequence>
       
<xsd:element ref="plm:ConstraintData" minOccurs="0"/>
       
<xsd:element ref="plm:ConstraintTargetRef" minOccurs="0" maxOccurs="unbounded"/>
       
<xsd:element ref="plm:JointData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:FrictionData" minOccurs="0" maxOccurs="2"/>
       
<xsd:element ref="plm:DriverData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:ForceData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:SpringData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:DamperData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:BushingData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:ContactData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:CouplerData" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:LimitsDependencyData" minOccurs="0" maxOccurs="1"/>
     
</xsd:sequence>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy