element ElectricalComponentUsage
diagram plmxml_diagrams/plmxml_p1785.png
namespace http://www.plmxml.org/Schemas/PLMXMLRouteListSchema
type routelist:ElectricalComponentUsageType
substitution group routelist:RouteListElement
properties
content complex
children plm:Description plm:ApplicationRef plm:UserData
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
uniqueId  xsd:normalizedString  required      
documentation
Unique identifier of the RouteList object.
componentRef  plm:anyURIType  required      
documentation
Refers to the electrical component for this usage.
instanceName  xsd:normalizedString  optional      
documentation
Physical part instance name or component name to which this logical component is assigned (or to be assigned)
assigned  derived by: xsd:NMTOKEN  optional      
documentation
This is an export only attribute.
Auto:  Automatically assigned to a physical component.
Manual: Manually assigned to a physical component.
Not Assigned: Not assigned to any physical component.
isRouted  xsd:boolean  optional      
documentation
This is an export only attribute.
True: Wire/Cable/SpaceReservations are routed to this component.
False: Wire/Cable/SpaceReservations are not routed to this component.
source <xsd:element name="ElectricalComponentUsage" type="routelist:ElectricalComponentUsageType" substitutionGroup="routelist:RouteListElement"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy