complexType FlowConnectionType
diagram plmxml_diagrams/plmxml_p995.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:ConnectionBase
properties
base plm:ConnectionBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:PropertyGroup
used by
element FlowConnection
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
catalogueId  xsd:string  optional      
optionRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
annotation
documentation

      This is a sub-class of Connection which corresponds to the AP212 Location,
      which "allows the flow of energy or information, for instance".
     
source <xsd:complexType name="FlowConnectionType">
 
<xsd:annotation>
   
<xsd:documentation>
      This is a sub-class of Connection which corresponds to the AP212 Location,
      which "allows the flow of energy or information, for instance".
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:ConnectionBase"/>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy