complexType GroupRuleEntryType
diagram plmxml_diagrams/plmxml_p1390.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:RuleEntryBase
properties
base plm:RuleEntryBase
children plm:Description plm:ApplicationRef plm:RuleEntry
used by
element GroupRuleEntry
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
annotation
documentation

      This RuleEntry contains subordinate RuleEntries, which are of equal precedence.
      They are all processed; if there is at least one match, then the revision with the
      most recent creation date is configured.
     
      SubElements:
     
      RuleEntry:        Each sub-element is a subordinate RuleEntry.
     
source <xsd:complexType name="GroupRuleEntryType">
 
<xsd:annotation>
   
<xsd:documentation>
      This RuleEntry contains subordinate RuleEntries, which are of equal precedence.
      They are all processed; if there is at least one match, then the revision with the
      most recent creation date is configured.
     
      SubElements:
     
      RuleEntry:        Each sub-element is a subordinate RuleEntry.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:RuleEntryBase">
     
<xsd:sequence>
       
<xsd:element ref="plm:RuleEntry" maxOccurs="unbounded"/>
     
</xsd:sequence>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy