complexType LimitsDependencyDataType
diagram plmxml_diagrams/plmxml_p869.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:AttribOwnerBase
properties
base plm:AttribOwnerBase
children plm:Description plm:ApplicationRef plm:Attribute plm:ValueWithUnit plm:RangeWithUnit
used by
element LimitsDependencyData
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
annotation
documentation

            Additional data for a Limits Dependency Constraint. Only one
            LimitsDependencyData sub-element is allowed in a Constraint,
            ConstraintInstance or ConstraintOccurrence element.

            Attributes:

            id:             Inherited from AttribOwner.
            name:           Inherited from AttribOwner.

            Sub-elements:

            ValueWithUnit:  The list of ValueWithUnit sub-elements represents
                            the values of the independent Joint given by the
                            first ConstraintTargetRef of the Limits Dependency.
                            The limits of the dependent Joint corresponding to a
                            given value are represented by the corresponding
                            RangeWithUnit sub-element. The limits of the
                            dependent Joint at intermediate values of the
                            independent Joint are found by linear interpolation.
            RangeWithUnit:  The list of RangeWithUnit sub-elements represents
                            the limits of the dependent Joint given by the
                            second ConstraintTargetRef of the Limits Dependency.
                            The value of the independent Joint corresponding to
                            given limits is represented by the corresponding
                            ValueWithUnit sub-element. The limits of the
                            dependent Joint at intermediate values of the
                            independent Joint are found by linear interpolation.
         
source <xsd:complexType name="LimitsDependencyDataType">
 
<xsd:annotation>
   
<xsd:documentation>
            Additional data for a Limits Dependency Constraint. Only one
            LimitsDependencyData sub-element is allowed in a Constraint,
            ConstraintInstance or ConstraintOccurrence element.

            Attributes:

            id:             Inherited from AttribOwner.
            name:           Inherited from AttribOwner.

            Sub-elements:

            ValueWithUnit:  The list of ValueWithUnit sub-elements represents
                            the values of the independent Joint given by the
                            first ConstraintTargetRef of the Limits Dependency.
                            The limits of the dependent Joint corresponding to a
                            given value are represented by the corresponding
                            RangeWithUnit sub-element. The limits of the
                            dependent Joint at intermediate values of the
                            independent Joint are found by linear interpolation.
            RangeWithUnit:  The list of RangeWithUnit sub-elements represents
                            the limits of the dependent Joint given by the
                            second ConstraintTargetRef of the Limits Dependency.
                            The value of the independent Joint corresponding to
                            given limits is represented by the corresponding
                            ValueWithUnit sub-element. The limits of the
                            dependent Joint at intermediate values of the
                            independent Joint are found by linear interpolation.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:AttribOwnerBase">
     
<xsd:sequence>
       
<xsd:element ref="plm:ValueWithUnit" minOccurs="0" maxOccurs="unbounded"/>
       
<xsd:element ref="plm:RangeWithUnit" minOccurs="0" maxOccurs="unbounded"/>
     
</xsd:sequence>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy