complexType MechanismInstanceType
diagram plmxml_diagrams/plmxml_p873.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:InstanceBase
properties
base plm:InstanceBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Transform plm:Representation plm:VariantCondition plm:Reference plm:PropertyGroup plm:EntityPropertyGroup plm:Marker
used by
element MechanismInstance
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
instancedRef  plm:anyURIType  optional      
transformRef  xsd:IDREF  optional      
materialRef  xsd:IDREF  optional      
partRef  plm:anyURIType  optional      
representationRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
designRequired  xsd:boolean  optional      
quantity  xsd:double  optional      
unitRef  xsd:IDREF  optional      
instanceType  xsd:string  optional      
sequenceNumber  xsd:nonNegativeInteger  optional      
instanceThreadRef  plm:anyURIType  optional      
instanceTypeRef  plm:anyURIType  optional      
annotation
documentation

            An Instance of a MechanismRevisionView. A MechanismInstance represents an instance of a
            Mechanism object.

            A MechanismInstance may reference geometry in the Product Structure via Reference elements. A
            Reference may reference an Occurrence in the Product Structure via its occurrenceRef attribute.
            A MechanismInstance may correspond to different Occurrence elements for different purposes by
            using more than one Reference. In this case, each Reference has a different value for its type
            attribute.

            Attributes:

            id:             Inherited from Instance.
            name:           Inherited from Instance.
            partRef:        Inherited from Instance. References a MechanismRevisionView, which represents a
                            Mechanism object.
            propertyRefs:   Inherited from Instance. A list of references to elements representing
                            properties such as mass or initial velocity. See also the PropertyGroup
                            sub-element. See the "Defining Mass and Material Properties" Chapter of the PLM
                            XML Schema Functional Description.

            Sub-elements:

            Bound:          Inherited from Instance. Represents the bounding box in which the Mechanism
                            object lies. See Section 5.4.2 of the PLM XML Schema Functional Description.
            PropertyGroup:  Inherited from Instance. May have sub-elements representing properties such as
                            mass or initial velocity. See also the propertyRefs attribute. See the
                            "Defining Mass and Material Properties" Chapter of the PLM XML Schema
                            Functional Description.
            Marker:         The Markers on the Mechanism object.
            Reference:      Inherited from Instance. The occurrenceRef attribute of a Reference element
                            references an Occurrence in the Product Structure. See the "Representing
                            Feature Semantics" Chapter of the PLM XML Schema Functional Description.
         
source <xsd:complexType name="MechanismInstanceType">
 
<xsd:annotation>
   
<xsd:documentation>
            An Instance of a MechanismRevisionView. A MechanismInstance represents an instance of a
            Mechanism object.

            A MechanismInstance may reference geometry in the Product Structure via Reference elements. A
            Reference may reference an Occurrence in the Product Structure via its occurrenceRef attribute.
            A MechanismInstance may correspond to different Occurrence elements for different purposes by
            using more than one Reference. In this case, each Reference has a different value for its type
            attribute.

            Attributes:

            id:             Inherited from Instance.
            name:           Inherited from Instance.
            partRef:        Inherited from Instance. References a MechanismRevisionView, which represents a
                            Mechanism object.
            propertyRefs:   Inherited from Instance. A list of references to elements representing
                            properties such as mass or initial velocity. See also the PropertyGroup
                            sub-element. See the "Defining Mass and Material Properties" Chapter of the PLM
                            XML Schema Functional Description.

            Sub-elements:

            Bound:          Inherited from Instance. Represents the bounding box in which the Mechanism
                            object lies. See Section 5.4.2 of the PLM XML Schema Functional Description.
            PropertyGroup:  Inherited from Instance. May have sub-elements representing properties such as
                            mass or initial velocity. See also the propertyRefs attribute. See the
                            "Defining Mass and Material Properties" Chapter of the PLM XML Schema
                            Functional Description.
            Marker:         The Markers on the Mechanism object.
            Reference:      Inherited from Instance. The occurrenceRef attribute of a Reference element
                            references an Occurrence in the Product Structure. See the "Representing
                            Feature Semantics" Chapter of the PLM XML Schema Functional Description.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:InstanceBase">
     
<xsd:choice minOccurs="0" maxOccurs="unbounded">
       
<xsd:element ref="plm:Marker"/>
     
</xsd:choice>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy