complexType MechanismOccurrenceType
diagram plmxml_diagrams/plmxml_p874.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:OccurrenceType
properties
base plm:OccurrenceType
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Transform plm:Representation plm:VariantCondition plm:Reference plm:PropertyGroup plm:EntityPropertyGroup plm:Material plm:EntityMaterial plm:AssociatedAttachment plm:AttributeContext plm:Marker
used by
element MechanismOccurrence
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
instancedRef  plm:anyURIType  optional      
transformRef  xsd:IDREF  optional      
materialRef  xsd:IDREF  optional      
partRef  plm:anyURIType  optional      
representationRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
designRequired  xsd:boolean  optional      
occurrenceRefs  xsd:IDREFS  optional      
instanceRefs  plm:uriReferenceListType  optional      
pathRefs  plm:uriReferenceListType  optional      
geometryRefs  plm:uriReferenceListType  optional      
alternativeOfRef  plm:anyURIType  optional      
productViewRef  plm:anyURIType  optional      
visible  xsd:boolean  optional      
lastInstanceParentRef  plm:anyURIType  optional      
sourceRef  plm:anyURIType  optional      
linkedOccurrenceRef  plm:anyURIType  optional      
linkedGroupRef  plm:anyURIType  optional      
associatedAttachmentRefs  plm:uriReferenceListType  optional      
parentRef  plm:anyURIType  optional      
instanceNumber  xsd:integer  optional      
occurrenceId  xsd:string  optional      
controlRefs  plm:uriReferenceListType  optional      
symbolicRefs  plm:uriReferenceListType  optional      
annotation
documentation

            An Occurrence of a MechanismRevisionView. A MechanismOccurrence represents an occurrence of a
            Mechanism object.

            A MechanismOccurrence may reference geometry in the Product Structure via Reference elements. A
            Reference may reference an Occurrence in the Product Structure via its occurrenceRef attribute.
            A MechanismOccurrence may correspond to different Occurrence elements for different purposes by
            using more than one Reference. In this case, each Reference has a different value for its type
            attribute.

            Attributes:

            id:             Inherited from Occurrence.
            name:           Inherited from Occurrence.
            instanceRefs:   Inherited from Occurrence. References a list of MechanismInstances, which
                            define a particular Mechanism object.
            propertyRefs:   Inherited from Occurrence. A list of references to elements representing
                            properties such as mass or initial velocity. See also the PropertyGroup
                            sub-element. See the "Defining Mass and Material Properties" Chapter of the PLM
                            XML Schema Functional Description.

            Sub-elements:

            Bound:          Inherited from Occurrence. Represents the bounding in which the Mechanism
                            object lies. See Section 5.4.2 of the PLM XML Schema Functional Description.
            PropertyGroup:  Inherited from Occurrence. May have sub-elements representing properties such
                            as mass or initial velocity. See also the propertyRefs attribute. See the
                            "Defining Mass and Material Properties" Chapter of the PLM XML Schema
                            Functional Description.
            Marker:         The Markers on the Mechanism object.
            Reference:      Inherited from Occurrence. The occurrenceRef attribute of a Reference element
                            references an Occurrence in the Product Structure. See the "Representing
                            Feature Semantics" Chapter of the PLM XML Schema Functional Description.
         
source <xsd:complexType name="MechanismOccurrenceType">
 
<xsd:annotation>
   
<xsd:documentation>
            An Occurrence of a MechanismRevisionView. A MechanismOccurrence represents an occurrence of a
            Mechanism object.

            A MechanismOccurrence may reference geometry in the Product Structure via Reference elements. A
            Reference may reference an Occurrence in the Product Structure via its occurrenceRef attribute.
            A MechanismOccurrence may correspond to different Occurrence elements for different purposes by
            using more than one Reference. In this case, each Reference has a different value for its type
            attribute.

            Attributes:

            id:             Inherited from Occurrence.
            name:           Inherited from Occurrence.
            instanceRefs:   Inherited from Occurrence. References a list of MechanismInstances, which
                            define a particular Mechanism object.
            propertyRefs:   Inherited from Occurrence. A list of references to elements representing
                            properties such as mass or initial velocity. See also the PropertyGroup
                            sub-element. See the "Defining Mass and Material Properties" Chapter of the PLM
                            XML Schema Functional Description.

            Sub-elements:

            Bound:          Inherited from Occurrence. Represents the bounding in which the Mechanism
                            object lies. See Section 5.4.2 of the PLM XML Schema Functional Description.
            PropertyGroup:  Inherited from Occurrence. May have sub-elements representing properties such
                            as mass or initial velocity. See also the propertyRefs attribute. See the
                            "Defining Mass and Material Properties" Chapter of the PLM XML Schema
                            Functional Description.
            Marker:         The Markers on the Mechanism object.
            Reference:      Inherited from Occurrence. The occurrenceRef attribute of a Reference element
                            references an Occurrence in the Product Structure. See the "Representing
                            Feature Semantics" Chapter of the PLM XML Schema Functional Description.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:OccurrenceType">
     
<xsd:choice minOccurs="0" maxOccurs="unbounded">
       
<xsd:element ref="plm:Marker"/>
     
</xsd:choice>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy