complexType MechanismRevisionViewType
diagram plmxml_diagrams/plmxml_p877.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:StructureRevisionViewBase
properties
base plm:StructureRevisionViewBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Occurrence plm:PropertyGroup plm:RepresentationEntity plm:EntityPropertyGroup plm:SymbolicOccurrence plm:MechanismParameters plm:Marker
used by
element MechanismRevisionView
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
revisionRef  plm:anyURIType  optional      
viewRef  plm:anyURIType  optional      
structureViewRef  plm:anyURIType  optional      
instanceRefs  xsd:IDREFS  optional      
gdeInstanceRefs  plm:uriReferenceListType  optional      
connectionInstanceRefs  plm:uriReferenceListType  optional      
signalInstanceRefs  plm:uriReferenceListType  optional      
routeInstanceRefs  plm:uriReferenceListType  optional      
occurrenceRefs  plm:uriReferenceListType  optional      
locationInstanceRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
ruleRefs  plm:uriReferenceListType  optional      
occurrenceControlState  plm:OccurrenceControlEnum    implicit    
annotation
documentation

            A view of a revision of a Mechanism, analogous to a ProductRevisionView in the Product
            Structure. MechanismRevisionView elements are used together with MechanismInstance elements in
            an instance graph. At the leaf nodes, they represent conceptual rigid bodies, which may be
            implemented by ProductRevisionView elements. At other levels, they represent sub-assemblies of
            conceptual rigid bodies, known as sub-mechanisms, and at the top level, they represent the
            mechanism definition.

            Attributes:

            id:             Inherited from StructureRevisionView.
            name:           Inherited from StructureRevisionView.
            instanceRefs:   Inherited from StructureRevisionView. References MechanismInstance elements,
                            which represent Mechanism objects.
            gdeInstanceRefs: Inherited from StructureRevisionView. References JointInstance elements.
            propertyRefs:   Inherited from StructureRevisionView. A list of references to elements
                            representing properties such as mass or initial velocity. See also the
                            PropertyGroup sub-element. See the "Defining Mass and Material Properties"
                            Chapter of the PLM XML Schema Functional Description.

            Sub-elements:

            Bound:          Inherited from StructureRevisionView. Represents the bounding box in which the
                            Mechanism object lies. See Section 5.4.2 of the PLM XML Schema Functional
                            Description.
            PropertyGroup:  Inherited from StructureRevisionView. May have sub-elements representing
                            properties such as mass or initial velocity. See also the propertyRefs
                            attribute. See the "Defining Mass and  Material Properties" Chapter of the PLM
                            XML Schema Functional Description.
            MechanismParameters: The parameters for a Mechanism solution.
            Marker:         The Markers on the Mechanism object.
         
source <xsd:complexType name="MechanismRevisionViewType">
 
<xsd:annotation>
   
<xsd:documentation>
            A view of a revision of a Mechanism, analogous to a ProductRevisionView in the Product
            Structure. MechanismRevisionView elements are used together with MechanismInstance elements in
            an instance graph. At the leaf nodes, they represent conceptual rigid bodies, which may be
            implemented by ProductRevisionView elements. At other levels, they represent sub-assemblies of
            conceptual rigid bodies, known as sub-mechanisms, and at the top level, they represent the
            mechanism definition.

            Attributes:

            id:             Inherited from StructureRevisionView.
            name:           Inherited from StructureRevisionView.
            instanceRefs:   Inherited from StructureRevisionView. References MechanismInstance elements,
                            which represent Mechanism objects.
            gdeInstanceRefs: Inherited from StructureRevisionView. References JointInstance elements.
            propertyRefs:   Inherited from StructureRevisionView. A list of references to elements
                            representing properties such as mass or initial velocity. See also the
                            PropertyGroup sub-element. See the "Defining Mass and Material Properties"
                            Chapter of the PLM XML Schema Functional Description.

            Sub-elements:

            Bound:          Inherited from StructureRevisionView. Represents the bounding box in which the
                            Mechanism object lies. See Section 5.4.2 of the PLM XML Schema Functional
                            Description.
            PropertyGroup:  Inherited from StructureRevisionView. May have sub-elements representing
                            properties such as mass or initial velocity. See also the propertyRefs
                            attribute. See the "Defining Mass and  Material Properties" Chapter of the PLM
                            XML Schema Functional Description.
            MechanismParameters: The parameters for a Mechanism solution.
            Marker:         The Markers on the Mechanism object.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:StructureRevisionViewBase">
     
<xsd:sequence>
       
<xsd:element ref="plm:MechanismParameters" minOccurs="0" maxOccurs="1"/>
       
<xsd:element ref="plm:Marker" minOccurs="0" maxOccurs="unbounded"/>
     
</xsd:sequence>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy