complexType MotionAssemblyType
diagram plmxml_diagrams/plmxml_p1043.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:AttribOwnerBase
properties
base plm:AttribOwnerBase
children plm:Description plm:ApplicationRef plm:Attribute plm:FrameSequenceInstance
used by
element MotionAssembly
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
annotation
documentation

            The container element for a sequence of FrameSequenceInstance
            elements.
           
            Sub-elements:
           
            FrameSequenceInstance: The instances of the FrameSequences in the
                            sequence.

         
source <xsd:complexType name="MotionAssemblyType">
 
<xsd:annotation>
   
<xsd:documentation>
            The container element for a sequence of FrameSequenceInstance
            elements.
           
            Sub-elements:
           
            FrameSequenceInstance: The instances of the FrameSequences in the
                            sequence.

         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:AttribOwnerBase">
     
<xsd:choice minOccurs="0" maxOccurs="unbounded">
       
<xsd:element ref="plm:FrameSequenceInstance"/>
     
</xsd:choice>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy