complexType OrType
diagram plmxml_diagrams/plmxml_p418.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:LogicalExpressionBase
properties
base plm:LogicalExpressionBase
children plm:LogicalExpression
used by
element Or
annotation
documentation

      Or - a type of logical expression.

      Elements:

      At least two sub-elements, derived from LogicalExpression. The Or expression
      returns true if any of its sub-elements return true.
     
source <xsd:complexType name="OrType">
 
<xsd:annotation>
   
<xsd:documentation>
      Or - a type of logical expression.

      Elements:

      At least two sub-elements, derived from LogicalExpression. The Or expression
      returns true if any of its sub-elements return true.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:LogicalExpressionBase">
     
<xsd:choice minOccurs="2" maxOccurs="unbounded">
       
<xsd:element ref="plm:LogicalExpression"/>
     
</xsd:choice>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy