element SpaceReservation
diagram plmxml_diagrams/plmxml_p1793.png
namespace http://www.plmxml.org/Schemas/PLMXMLRouteListSchema
type routelist:SpaceReservationType
substitution group routelist:RouteListElement
properties
content complex
children plm:Description plm:ApplicationRef
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
crossSectionType  routelist:CrossSectionType    circular    
documentation
Cable cross-section type (Circular, flat). If no cross section type is specified then the type is set to Circular.
outerDiameter  xsd:double  optional      
documentation
Outer diameter of the space-reservation. If is ignored if the cross-section type is flat.
height  xsd:double  optional      
documentation
Height of the space-reservation. It is ignored if the cross-section type is circular.
width  xsd:double  optional      
documentation
Width of the space-reservation. It is ignored if the cross-section type is circular
multiplier  xsd:double  optional      
documentation
A factor used as a multiplier on the actual length to calculate the cut-length.
offset  xsd:double  optional      
documentation
A value used to calculate the cut-length by adding it to the actual length after the multiplier is applied.
source <xsd:element name="SpaceReservation" type="routelist:SpaceReservationType" substitutionGroup="routelist:RouteListElement"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy