complexType YieldStressType
diagram plmxml_diagrams/plmxml_p570.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:PropertyBase
properties
base plm:PropertyBase
children plm:Description plm:ApplicationRef plm:Attribute plm:ValueWithUnit plm:RangeWithUnit
used by
element YieldStress
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
ownerRef  plm:anyURIType  optional      
annotation
documentation

      This Property gives the Yield Stress of an object (the tensile stress a
      material can support without permanent deformation).
     
      Elements:
     
      ValueWithUnit
      RangeWithUnit  one of these sub-elements should be used to indicate the value
                     or range of the Property.
     
source <xsd:complexType name="YieldStressType">
 
<xsd:annotation>
   
<xsd:documentation>
      This Property gives the Yield Stress of an object (the tensile stress a
      material can support without permanent deformation).
     
      Elements:
     
      ValueWithUnit
      RangeWithUnit  one of these sub-elements should be used to indicate the value
                     or range of the Property.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:PropertyBase">
     
<xsd:choice>
       
<xsd:element ref="plm:ValueWithUnit"/>
       
<xsd:element ref="plm:RangeWithUnit"/>
     
</xsd:choice>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy