| Name | Type | Use | Default | Fixed | Annotation |
| id | xsd:ID | optional | | | |
| name | xsd:string | optional | | | |
| nameRef | plm:anyURIType | optional | | | |
| descriptionTextRef | plm:anyURIType | optional | | | |
| uniqueId | xsd:normalizedString | required | | | | documentation | | Unique identifier of the RouteList object. |
|
| conductorRef | plm:anyURIType | required | | | | documentation | | Reference to Wire, Cable, or Space Reservation element. The resolution is based on the Type. |
|
| wireClass | derived by: xsd:NMTOKEN | optional | | | |
| wireSignal | xsd:normalizedString | optional | | | |
| wireSeparationCode | xsd:normalizedString | optional | | | |
| location | xsd:integer | optional | | | | documentation | Location of the assigned conductor.
(1. Ordering of the wire in a flat cable
2. Ordering of the cable in a stacked flat cables.) |
|
| length | xsd:double | optional | | | | documentation | | Length of the connection. This is export only field from UG-NX. |
|
| cutLength | xsd:double | optional | | | | documentation |
Cut length calculated based on the offset and
multiplier defined by the assigned conductor (Wire,
Cable, Space reservation). This is export only.
|
|
| routed | derived by: xsd:NMTOKEN | optional | | | | documentation | This is export only field
Auto - Routed automatically
Manual - Routed Manually
Not Routed |
|
| harnessRef | plm:anyURIType | optional | | | | documentation | | Reference to the Harness to which the wire/cable/space-reservation occurance belongs. |
|