| diagram | ![]() |
||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||
| type | extension of plm:OccurrenceType | ||
| properties |
|
||
| children | plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Transform plm:Representation plm:VariantCondition plm:Reference plm:PropertyGroup plm:EntityPropertyGroup plm:Material plm:EntityMaterial plm:AssociatedAttachment plm:AttributeContext plm:ConstraintData plm:ConstraintTargetRef plm:JointData plm:FrictionData plm:DriverData plm:ForceData plm:SpringData plm:DamperData plm:BushingData plm:ContactData plm:CouplerData plm:LimitsDependencyData | ||
| used by |
|
||
| attributes | |||
| annotation |
|
||
| source | <xsd:complexType name="ConstraintOccurrenceType"> <xsd:annotation> <xsd:documentation> This subclass of Occurrence may be used where the Occurrence references a Constraint. If a particular type of sub-element is present, the ConstraintOccurrence overrides the entire set of sub-elements of that type present under the ConstraintInstance or Constraint. Sub-elements: ConstraintData: Overrides the data defining the geometric Constraint or the Contact Constraint. ConstraintTargetRef: Overrides references to constrained geometry. JointData: Overrides additional data for a Joint Constraint. FrictionData: Overrides additional data for a Friction Constraint or a Joint Constraint. DriverData: Overrides additional data for a Driver Constraint or a Joint Constraint. ForceData: Overrides additional data for a Force Constraint. SpringData: Overrides additional data for a Spring Constraint. DamperData: Overrides additional data for a Damper Constraint. BushingData: Overrides additional data for a Bushing Constraint. ContactData: Overrides additional data for a Contact Constraint. CouplerData: Overrides additional data for a Coupler Constraint or a Joint Constraint that infers a Joint. LimitsDependencyData: Additional data for a Limits Dependency Constraint. </xsd:documentation> </xsd:annotation> <xsd:complexContent> <xsd:extension base="plm:OccurrenceType"> <xsd:sequence> <xsd:element ref="plm:ConstraintData" minOccurs="0"/> <xsd:element ref="plm:ConstraintTargetRef" minOccurs="0" maxOccurs="unbounded"/> <xsd:element ref="plm:JointData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:FrictionData" minOccurs="0" maxOccurs="2"/> <xsd:element ref="plm:DriverData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:ForceData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:SpringData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:DamperData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:BushingData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:ContactData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:CouplerData" minOccurs="0" maxOccurs="1"/> <xsd:element ref="plm:LimitsDependencyData" minOccurs="0" maxOccurs="1"/> </xsd:sequence> </xsd:extension> </xsd:complexContent> </xsd:complexType> |