| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| type | restriction of xsd:string | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| used by |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| facets |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| annotation |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:simpleType name="GDERelationshipType"> <xsd:annotation> <xsd:documentation> This is the type of a relationship between two Occurrences or Instances. associated: attached: related: connection: An Occurrence of a Connection, related to an Occurrence of a GDE to which it connects. implementation: An 'implemented by' relation, for example between an Occurrence of a Connection and an Occurrence of a ProductRevisionView; or between an Occurrence of a functional PRV and a physical PRV. implements: The inverse of 'implemented by'. For example, an Occurrence of a PRV may implement a RouteSection. realisation: misc: signalSource: from Instance of a Signal to Occurrence of a Signal, Connection, GDE or Product. signalTarget: from Instance of a Signal to Occurrence of a Signal, Connection, GDE or Product. signalTransmitter: from Instance of a Signal to Occurrence of a Signal, Connection, GDE or Product. processVariable: from Instance of a Signal to the corresponding Occurrence of a ProcessVariable. redundancy: from Instance of Signal to Occurrence of a Signal which is replicated by the first one. signalValue: from Instance of a Signal to a SignalValue. processVariableValue: from Instance of a ProcessVariable to a ValueWithUnit. route: from an Occurrence or Instance to a Route. software: from an Occurrence or Instance of a Processor or Software to an Occurrence or Instance of a Software which uses or depends on it. processorGateway: from an Occurrence or Instance of a Processor to an Occurrence or Instance of another Processor for which the first Processor acts as a Gateway. mass: Relates a MechanismOccurrence or MechanismInstance to an Occurrence or Instance in the ProductStructure that determines its mass. sharedAssociated: References shared geometry. </xsd:documentation> </xsd:annotation> <xsd:restriction base="xsd:string"> <xsd:enumeration value="associated"/> <xsd:enumeration value="attached"/> <xsd:enumeration value="related"/> <xsd:enumeration value="connection"/> <xsd:enumeration value="implementation"/> <xsd:enumeration value="implements"/> <xsd:enumeration value="realisation"/> <xsd:enumeration value="misc"/> <xsd:enumeration value="signalSource"/> <xsd:enumeration value="signalTarget"/> <xsd:enumeration value="signalTransmitter"/> <xsd:enumeration value="processVariable"/> <xsd:enumeration value="redundancy"/> <xsd:enumeration value="signalValue"/> <xsd:enumeration value="processVariableValue"/> <xsd:enumeration value="route"/> <xsd:enumeration value="software"/> <xsd:enumeration value="processorGateway"/> <xsd:enumeration value="mass"/> <xsd:enumeration value="sharedAssociated"/> </xsd:restriction> </xsd:simpleType> |