| Name | Type | Use | Default | Fixed | Annotation |
| id | xsd:ID | optional | | | |
| name | xsd:string | optional | | | |
| nameRef | plm:anyURIType | optional | | | |
| descriptionTextRef | plm:anyURIType | optional | | | |
| uniqueId | xsd:normalizedString | required | | | | documentation | | Unique identifier of the RouteList object. |
|
| componentRef | plm:anyURIType | required | | | | documentation | | Refers to the electrical component for this usage. |
|
| instanceName | xsd:normalizedString | optional | | | | documentation | | Physical part instance name or component name to which this logical component is assigned (or to be assigned) |
|
| assigned | derived by: xsd:NMTOKEN | optional | | | | documentation | This is an export only attribute.
Auto: Automatically assigned to a physical component.
Manual: Manually assigned to a physical component.
Not Assigned: Not assigned to any physical component. |
|
| isRouted | xsd:boolean | optional | | | | documentation | This is an export only attribute.
True: Wire/Cable/SpaceReservations are routed to this component.
False: Wire/Cable/SpaceReservations are not routed to this component. |
|
| type | derived by: xsd:NMTOKEN | | connector | | | documentation | | Type of the Harness Component (Connector/Splice). If no type is specified then the type is set Connector. |
|
| nonHarnessComponentRef | plm:anyURIType | optional | | | | documentation | | Refers to the device to which connector or splice is attached. |
|