| diagram | ![]() |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| type | extension of plm:InstanceBase | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| children | plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Transform plm:Representation plm:VariantCondition plm:Reference plm:PropertyGroup plm:EntityPropertyGroup plm:Marker | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| used by |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| attributes |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| annotation |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:complexType name="MechanismInstanceType"> <xsd:annotation> <xsd:documentation> An Instance of a MechanismRevisionView. A MechanismInstance represents an instance of a Mechanism object. A MechanismInstance may reference geometry in the Product Structure via Reference elements. A Reference may reference an Occurrence in the Product Structure via its occurrenceRef attribute. A MechanismInstance may correspond to different Occurrence elements for different purposes by using more than one Reference. In this case, each Reference has a different value for its type attribute. Attributes: id: Inherited from Instance. name: Inherited from Instance. partRef: Inherited from Instance. References a MechanismRevisionView, which represents a Mechanism object. propertyRefs: Inherited from Instance. A list of references to elements representing properties such as mass or initial velocity. See also the PropertyGroup sub-element. See the "Defining Mass and Material Properties" Chapter of the PLM XML Schema Functional Description. Sub-elements: Bound: Inherited from Instance. Represents the bounding box in which the Mechanism object lies. See Section 5.4.2 of the PLM XML Schema Functional Description. PropertyGroup: Inherited from Instance. May have sub-elements representing properties such as mass or initial velocity. See also the propertyRefs attribute. See the "Defining Mass and Material Properties" Chapter of the PLM XML Schema Functional Description. Marker: The Markers on the Mechanism object. Reference: Inherited from Instance. The occurrenceRef attribute of a Reference element references an Occurrence in the Product Structure. See the "Representing Feature Semantics" Chapter of the PLM XML Schema Functional Description. </xsd:documentation> </xsd:annotation> <xsd:complexContent> <xsd:extension base="plm:InstanceBase"> <xsd:choice minOccurs="0" maxOccurs="unbounded"> <xsd:element ref="plm:Marker"/> </xsd:choice> </xsd:extension> </xsd:complexContent> </xsd:complexType> |