complexType ApplicationInterfaceType
diagram plmxml_diagrams/plmxml_p1570.png
namespace http://www.plmxml.org/Schemas/PLMXMLBusinessSchema
type extension of bus:BusinessDataDefBase
properties
base bus:BusinessDataDefBase
children plm:Description plm:ApplicationRef plm:Attribute
used by
element ApplicationInterface
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
incrementalChangeRequired  xsd:boolean  optional      
objectTypes  xsd:string  optional      
viewRefs  plm:uriReferenceListType  optional      
exportTransferModeRef  plm:anyURIType  optional      
importTransferModeRef  plm:anyURIType  optional      
toolRef  plm:anyURIType  optional      
annotation
documentation

      This element describes the integration between the main application and an
      external application.
     
      Attributes:    
                     
      incrementalChangeRequired: If "true", this means that when the external application
                           makes changes to data sent from the main app, these changes
                           must be recorded in the main database under an Incremental Change.
     
      objectTypes:         This is an array of types, which defines the object types understood
                           by the external application.
      viewRefs:            This is an array of View elements giving the Views which the application
                           is allowed to access/process.
      exportTransferModeRef: This is the TransferMode used to export PLM XML to the external application.
      importTransferModeRef: This is the TransferMode used to import PLM XML from the external application.
      toolRef:             This specifies the ApplicationToolDef element which corresponds to
                           the external application.
     
source <xsd:complexType name="ApplicationInterfaceType">
 
<xsd:annotation>
   
<xsd:documentation>
      This element describes the integration between the main application and an
      external application.
     
      Attributes:    
                     
      incrementalChangeRequired: If "true", this means that when the external application
                           makes changes to data sent from the main app, these changes
                           must be recorded in the main database under an Incremental Change.
     
      objectTypes:         This is an array of types, which defines the object types understood
                           by the external application.
      viewRefs:            This is an array of View elements giving the Views which the application
                           is allowed to access/process.
      exportTransferModeRef: This is the TransferMode used to export PLM XML to the external application.
      importTransferModeRef: This is the TransferMode used to import PLM XML from the external application.
      toolRef:             This specifies the ApplicationToolDef element which corresponds to
                           the external application.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="bus:BusinessDataDefBase">
     
<xsd:attribute name="incrementalChangeRequired" type="xsd:boolean" use="optional"/>
     
<xsd:attribute name="objectTypes" type="xsd:string" use="optional"/>
     
<xsd:attribute name="viewRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:View"/>
     
<xsd:attribute name="exportTransferModeRef" type="plm:anyURIType" use="optional" plm:refType="bus:TransferMode"/>
     
<xsd:attribute name="importTransferModeRef" type="plm:anyURIType" use="optional" plm:refType="bus:TransferMode"/>
     
<xsd:attribute name="toolRef" type="plm:anyURIType" use="optional" plm:refType="bus:ApplicationToolDef"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute ApplicationInterfaceType/@incrementalChangeRequired
type xsd:boolean
properties
use optional
source <xsd:attribute name="incrementalChangeRequired" type="xsd:boolean" use="optional"/>

attribute ApplicationInterfaceType/@objectTypes
type xsd:string
properties
use optional
source <xsd:attribute name="objectTypes" type="xsd:string" use="optional"/>

attribute ApplicationInterfaceType/@viewRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="viewRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:View"/>

attribute ApplicationInterfaceType/@exportTransferModeRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="exportTransferModeRef" type="plm:anyURIType" use="optional" plm:refType="bus:TransferMode"/>

attribute ApplicationInterfaceType/@importTransferModeRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="importTransferModeRef" type="plm:anyURIType" use="optional" plm:refType="bus:TransferMode"/>

attribute ApplicationInterfaceType/@toolRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="toolRef" type="plm:anyURIType" use="optional" plm:refType="bus:ApplicationToolDef"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy