diagram | ![]() |
||||||||||||||||||||||||
namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||
used by |
|
||||||||||||||||||||||||
attributes |
|
||||||||||||||||||||||||
annotation |
|
||||||||||||||||||||||||
source | <xsd:complexType name="ApplicationRefType"> <xsd:annotation> <xsd:documentation> The ApplicationRef element is meant to relate the parent element (Product, Representation, etc) back to the owning entity in the sending application. Attributes: application: the context in which the contents of the label and version attributes make sense. Whether this field includes an application version number is up to the application, as long as it starts with something identifiable to the sending application. label: the string which identifies the application entity - the value of this field is only meaningful to the sending/authoring application. The receiving application can compare the contents of the attribute to test if two entities are the 'same' entity. But the actual value is meaningless to the receiving application. version: the optional string attribute which identifies the version of the application entity. This attribute can only be used to test if the versions of an entity are the same (i.e. the test is only meaningful if the label attribute values are the same). No version ordering can be deduced from the value. Similar to the label attribute, the version attribute contents are meaningless to the receiving application. </xsd:documentation> </xsd:annotation> <xsd:attribute name="application" type="xsd:string" use="optional"/> <xsd:attribute name="label" type="xsd:string" use="required"/> <xsd:attribute name="version" type="xsd:string" use="optional"/> </xsd:complexType> |
type | xsd:string | ||
properties |
|
||
source | <xsd:attribute name="application" type="xsd:string" use="optional"/> |
type | xsd:string | ||
properties |
|
||
source | <xsd:attribute name="label" type="xsd:string" use="required"/> |
type | xsd:string | ||
properties |
|
||
source | <xsd:attribute name="version" type="xsd:string" use="optional"/> |