complexType AssociatedAttachmentType
diagram plmxml_diagrams/plmxml_p221.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:AttribOwnerBase
properties
base plm:AttribOwnerBase
children plm:Description plm:ApplicationRef plm:Attribute
used by
element AssociatedAttachment
complexType ConfiguredActivityType
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
role  xsd:string        
contextRef  plm:anyURIType        
attachmentRef  plm:anyURIType  required      
childRefs  plm:uriReferenceListType        
roleRef  plm:anyURIType  optional      
annotation
documentation

      Represents a configured attachment to an Occurrence. When an unconfigured
      element (such as a ProductInstance) has an attachment, for example by
      means of a GeneralRelation, or AssociatedDataSet, then a corresponding
      configured element (such as an Occurrence) may have that attachment
      configured.

      Attributes:

      role:             the role of the attachment i.e. the relation to its owner.
      contextRef:       The corresponding configured element (e.g.
                        ProductInstance) which owns the attachment.
      attachmentRef:    reference to the attached element.
      childRefs:        sub-Attachments
      roleRef:          References a multiple language version of role. If
                        multiple language support is required, roleRef should be
                        used in addition to role.
     
source <xsd:complexType name="AssociatedAttachmentType">
 
<xsd:annotation>
   
<xsd:documentation>
      Represents a configured attachment to an Occurrence. When an unconfigured
      element (such as a ProductInstance) has an attachment, for example by
      means of a GeneralRelation, or AssociatedDataSet, then a corresponding
      configured element (such as an Occurrence) may have that attachment
      configured.

      Attributes:

      role:             the role of the attachment i.e. the relation to its owner.
      contextRef:       The corresponding configured element (e.g.
                        ProductInstance) which owns the attachment.
      attachmentRef:    reference to the attached element.
      childRefs:        sub-Attachments
      roleRef:          References a multiple language version of role. If
                        multiple language support is required, roleRef should be
                        used in addition to role.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:AttribOwnerBase">
     
<xsd:attribute name="role" type="xsd:string"/>
     
<xsd:attribute name="contextRef" type="plm:anyURIType"/>
     
<xsd:attribute name="attachmentRef" type="plm:anyURIType" use="required"/>
     
<xsd:attribute name="childRefs" type="plm:uriReferenceListType" plm:refType="plm:AssociatedAttachment"/>
     
<xsd:attribute name="roleRef" type="plm:anyURIType" use="optional" plm:refType="plm:Text"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute AssociatedAttachmentType/@role
type xsd:string
source <xsd:attribute name="role" type="xsd:string"/>

attribute AssociatedAttachmentType/@contextRef
type plm:anyURIType
source <xsd:attribute name="contextRef" type="plm:anyURIType"/>

attribute AssociatedAttachmentType/@attachmentRef
type plm:anyURIType
properties
use required
source <xsd:attribute name="attachmentRef" type="plm:anyURIType" use="required"/>

attribute AssociatedAttachmentType/@childRefs
type plm:uriReferenceListType
source <xsd:attribute name="childRefs" type="plm:uriReferenceListType" plm:refType="plm:AssociatedAttachment"/>

attribute AssociatedAttachmentType/@roleRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="roleRef" type="plm:anyURIType" use="optional" plm:refType="plm:Text"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy