complexType ConstraintDataType
diagram plmxml_diagrams/plmxml_p841.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:IdBase
properties
base plm:IdBase
used by
element ConstraintData
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
value  xsd:double  optional      
dimension  plm:DimensionalityType    3    
orientation  plm:ConstraintAlignmentEnum  optional      
alignment  plm:ConstraintAlignmentEnum  optional      
torusCoincidence  plm:ConstraintTorusCoincidenceEnum  optional      
suppressed  xsd:boolean  optional      
rigid  xsd:boolean  optional      
annotation
documentation

            A ConstraintData element contains information which defines a constraint.

            Attributes:

            value:          the numerical value of the constraint, in metres or radians.
            dimension:      whether a 2- or 3-dimensional constraint.
            orientation:    surface orientation - "align" or "antiAlign"
            alignment:      direction alignment - "align" or "antiAlign"
            torusCoincidence: additional information for when the constraint involves coincidence with a
                            torus.
            suppressed:     true if this constraint is not to be used when solving the system of
                            constraints.
            rigid:          true if the constraint is "rigid", i.e. it is not necessarily possible to vary
                            the value of the constraint while fixing the values of all the other
                            constraints.
         
source <xsd:complexType name="ConstraintDataType">
 
<xsd:annotation>
   
<xsd:documentation>
            A ConstraintData element contains information which defines a constraint.

            Attributes:

            value:          the numerical value of the constraint, in metres or radians.
            dimension:      whether a 2- or 3-dimensional constraint.
            orientation:    surface orientation - "align" or "antiAlign"
            alignment:      direction alignment - "align" or "antiAlign"
            torusCoincidence: additional information for when the constraint involves coincidence with a
                            torus.
            suppressed:     true if this constraint is not to be used when solving the system of
                            constraints.
            rigid:          true if the constraint is "rigid", i.e. it is not necessarily possible to vary
                            the value of the constraint while fixing the values of all the other
                            constraints.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:IdBase">
     
<xsd:attribute name="value" type="xsd:double" use="optional"/>
     
<xsd:attribute name="dimension" type="plm:DimensionalityType" default="3"/>
     
<xsd:attribute name="orientation" type="plm:ConstraintAlignmentEnum" use="optional"/>
     
<xsd:attribute name="alignment" type="plm:ConstraintAlignmentEnum" use="optional"/>
     
<xsd:attribute name="torusCoincidence" type="plm:ConstraintTorusCoincidenceEnum" use="optional"/>
     
<xsd:attribute name="suppressed" type="xsd:boolean" use="optional"/>
     
<xsd:attribute name="rigid" type="xsd:boolean" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute ConstraintDataType/@value
type xsd:double
properties
use optional
source <xsd:attribute name="value" type="xsd:double" use="optional"/>

attribute ConstraintDataType/@dimension
type plm:DimensionalityType
properties
default 3
facets
Kind Value Annotation
minInclusive 2
maxInclusive 3
source <xsd:attribute name="dimension" type="plm:DimensionalityType" default="3"/>

attribute ConstraintDataType/@orientation
type plm:ConstraintAlignmentEnum
properties
use optional
facets
Kind Value Annotation
enumeration align
enumeration antiAlign
source <xsd:attribute name="orientation" type="plm:ConstraintAlignmentEnum" use="optional"/>

attribute ConstraintDataType/@alignment
type plm:ConstraintAlignmentEnum
properties
use optional
facets
Kind Value Annotation
enumeration align
enumeration antiAlign
source <xsd:attribute name="alignment" type="plm:ConstraintAlignmentEnum" use="optional"/>

attribute ConstraintDataType/@torusCoincidence
type plm:ConstraintTorusCoincidenceEnum
properties
use optional
facets
Kind Value Annotation
enumeration coincident
enumeration coincidentWithSpine
enumeration coincidentAroundSpine
source <xsd:attribute name="torusCoincidence" type="plm:ConstraintTorusCoincidenceEnum" use="optional"/>

attribute ConstraintDataType/@suppressed
type xsd:boolean
properties
use optional
source <xsd:attribute name="suppressed" type="xsd:boolean" use="optional"/>

attribute ConstraintDataType/@rigid
type xsd:boolean
properties
use optional
source <xsd:attribute name="rigid" type="xsd:boolean" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy