complexType ConstraintTargetRefType
diagram plmxml_diagrams/plmxml_p845.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:GDEReferenceType
properties
base plm:GDEReferenceType
children plm:Description plm:ApplicationRef plm:Attribute plm:EntityRef plm:ConstraintHelp plm:GeometryData
used by
element ConstraintTargetRef
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
type  plm:GDERelationshipType  optional      
occurrenceRef  plm:anyURIType  optional      
targetRef  plm:anyURIType  optional      
pathRefs  plm:uriReferenceListType  optional      
halfSpace  plm:ConstraintHalfSpaceEnum  optional      
degreeOfFreedom  plm:DegreeOfFreedomEnum  optional      
annotation
documentation

            A ConstraintTargetRef is a means of referencing the target of a constraint, typically a
            geometric object, together with associated information required by the constraint. It uses the
            "occurrenceRef" attribute, and "EntityRef" sub-element, inherited from GDEReferenceType.

            Attributes:

            halfSpace:      specifies the relevant halfspace of the geometry.
            occurrenceRef:  Inherited from GDEReference. References a MechanismOccurrence. See the
                            "Representing Feature Semantics" Chapter of the PLM XML Schema Functional
                            Description.
            pathRefs:       Inherited from GDEReference. References a list of MechanismInstances, which
                            defines an occurrence of a Mechanism object by defining a unique path through
                            an instance graph.
            targetRef:      Inherited from GDEReference. References the target Marker, Joint or geometry.
            degreeOfFreedom: If the target of the constraint is a Joint, degreeOfFreedom specifies the
                            degree of freedom of the Joint that the ConstraintTargetRef targets.

            Sub-elements:

            ConstraintHelp: an element derived from ConstraintHelp, which assists the constraint solver.
            GeometryData:   If the target is geometry, GeometryData contains information about the
                            geometric object.
         
source <xsd:complexType name="ConstraintTargetRefType">
 
<xsd:annotation>
   
<xsd:documentation>
            A ConstraintTargetRef is a means of referencing the target of a constraint, typically a
            geometric object, together with associated information required by the constraint. It uses the
            "occurrenceRef" attribute, and "EntityRef" sub-element, inherited from GDEReferenceType.

            Attributes:

            halfSpace:      specifies the relevant halfspace of the geometry.
            occurrenceRef:  Inherited from GDEReference. References a MechanismOccurrence. See the
                            "Representing Feature Semantics" Chapter of the PLM XML Schema Functional
                            Description.
            pathRefs:       Inherited from GDEReference. References a list of MechanismInstances, which
                            defines an occurrence of a Mechanism object by defining a unique path through
                            an instance graph.
            targetRef:      Inherited from GDEReference. References the target Marker, Joint or geometry.
            degreeOfFreedom: If the target of the constraint is a Joint, degreeOfFreedom specifies the
                            degree of freedom of the Joint that the ConstraintTargetRef targets.

            Sub-elements:

            ConstraintHelp: an element derived from ConstraintHelp, which assists the constraint solver.
            GeometryData:   If the target is geometry, GeometryData contains information about the
                            geometric object.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:GDEReferenceType">
     
<xsd:sequence>
       
<xsd:element ref="plm:ConstraintHelp" minOccurs="0"/>
       
<xsd:element ref="plm:GeometryData" minOccurs="0"/>
     
</xsd:sequence>
     
<xsd:attribute name="halfSpace" type="plm:ConstraintHalfSpaceEnum" use="optional"/>
     
<xsd:attribute name="degreeOfFreedom" type="plm:DegreeOfFreedomEnum" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute ConstraintTargetRefType/@halfSpace
type plm:ConstraintHalfSpaceEnum
properties
use optional
facets
Kind Value Annotation
enumeration positive
enumeration negative
source <xsd:attribute name="halfSpace" type="plm:ConstraintHalfSpaceEnum" use="optional"/>

attribute ConstraintTargetRefType/@degreeOfFreedom
type plm:DegreeOfFreedomEnum
properties
use optional
facets
Kind Value Annotation
enumeration x
enumeration y
enumeration z
enumeration rx
enumeration ry
enumeration rz
source <xsd:attribute name="degreeOfFreedom" type="plm:DegreeOfFreedomEnum" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy