complexType DeepCopyRuleType
diagram plmxml_diagrams/plmxml_p1589.png
namespace http://www.plmxml.org/Schemas/PLMXMLBusinessSchema
type extension of bus:BusinessRuleBase
properties
base bus:BusinessRuleBase
children plm:Description plm:ApplicationRef plm:Attribute
used by
element DeepCopyRule
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
isExportable  xsd:boolean  optional  true    
isReplaceable  xsd:boolean  optional  true    
version  xsd:string  optional      
typeName  xsd:string  required      
operation  bus:DeepCopyRuleOperationType  required      
copyType  bus:DeepCopyType  required      
relationType  xsd:string  required      
attachmentType  xsd:string  required      
isRequired  xsd:boolean  optional      
annotation
documentation

      This element contains a Business rule of Type Deep Copy Rule. When doing a Save As
      or Revise, specifies what should be copied forward as a physical copy or reference
      or not copied forward at all.

      Attributes:
     
      typeName:              Object Type on which this rule applies
      operation:             Whether it is SaveAs or Revise
      copyType:
      relationType:
      attachmentType:
      isRequired:
     
source <xsd:complexType name="DeepCopyRuleType">
 
<xsd:annotation>
   
<xsd:documentation xml:lang="en">
      This element contains a Business rule of Type Deep Copy Rule. When doing a Save As
      or Revise, specifies what should be copied forward as a physical copy or reference
      or not copied forward at all.

      Attributes:
     
      typeName:              Object Type on which this rule applies
      operation:             Whether it is SaveAs or Revise
      copyType:
      relationType:
      attachmentType:
      isRequired:
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="bus:BusinessRuleBase">
     
<xsd:attribute name="typeName" type="xsd:string" use="required"/>
     
<xsd:attribute name="operation" type="bus:DeepCopyRuleOperationType" use="required"/>
     
<xsd:attribute name="copyType" type="bus:DeepCopyType" use="required"/>
     
<xsd:attribute name="relationType" type="xsd:string" use="required"/>
     
<xsd:attribute name="attachmentType" type="xsd:string" use="required"/>
     
<xsd:attribute name="isRequired" type="xsd:boolean" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute DeepCopyRuleType/@typeName
type xsd:string
properties
use required
source <xsd:attribute name="typeName" type="xsd:string" use="required"/>

attribute DeepCopyRuleType/@operation
type bus:DeepCopyRuleOperationType
properties
use required
facets
Kind Value Annotation
enumeration saveAs
enumeration revise
source <xsd:attribute name="operation" type="bus:DeepCopyRuleOperationType" use="required"/>

attribute DeepCopyRuleType/@copyType
type bus:DeepCopyType
properties
use required
facets
Kind Value Annotation
enumeration copyAsObject
enumeration copyAsReference
enumeration noCopy
source <xsd:attribute name="copyType" type="bus:DeepCopyType" use="required"/>

attribute DeepCopyRuleType/@relationType
type xsd:string
properties
use required
source <xsd:attribute name="relationType" type="xsd:string" use="required"/>

attribute DeepCopyRuleType/@attachmentType
type xsd:string
properties
use required
source <xsd:attribute name="attachmentType" type="xsd:string" use="required"/>

attribute DeepCopyRuleType/@isRequired
type xsd:boolean
properties
use optional
source <xsd:attribute name="isRequired" type="xsd:boolean" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy