complexType DeltaAddType
diagram plmxml_diagrams/plmxml_p896.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:DeltaOperationBase
properties
base plm:DeltaOperationBase
mixed true
used by
elements DeltaOperationGroupType/Add PLMXMLDeltaType/Add
attributes
Name  Type  Use  Default  Fixed  Annotation
parentRef  plm:anyURIType  optional      
siblingRef  plm:anyURIType  optional      
annotation
documentation

      This element represents adding a fragment of PLMXML, i.e. a tree of elements, to
      a master document.
     
      The sub-elements of this element are all added.
     
      Attributes:
     
      parentRef:       A URI reference to a placeholder element which represents the
                       element in the master document which will become the parent of the
                       added elements. Exactly one of parentRef or siblingRef should be present.
                      
      siblingRef:      A URI reference to a placeholder element which represents the
                       element in the master document which will become a sibling
                       of the added elements. There is no implication that the added element
                       will be adjacent to the sibling element in the sub-element ordering -
                       only that it will have the same parent.
     
      Elements:
     
      Any PLMXML elements may be included as sub-elements.
     
appinfo
allowMixed=true
source <xsd:complexType name="DeltaAddType" mixed="true">
 
<xsd:annotation>
   
<xsd:documentation>
      This element represents adding a fragment of PLMXML, i.e. a tree of elements, to
      a master document.
     
      The sub-elements of this element are all added.
     
      Attributes:
     
      parentRef:       A URI reference to a placeholder element which represents the
                       element in the master document which will become the parent of the
                       added elements. Exactly one of parentRef or siblingRef should be present.
                      
      siblingRef:      A URI reference to a placeholder element which represents the
                       element in the master document which will become a sibling
                       of the added elements. There is no implication that the added element
                       will be adjacent to the sibling element in the sub-element ordering -
                       only that it will have the same parent.
     
      Elements:
     
      Any PLMXML elements may be included as sub-elements.
     
</xsd:documentation>
   
<xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=true</xsd:appinfo>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:DeltaOperationBase">
     
<xsd:sequence>
       
<xsd:any namespace="##any" processContents="skip" maxOccurs="unbounded"/>
     
</xsd:sequence>
     
<xsd:attribute name="parentRef" type="plm:anyURIType" use="optional"/>
     
<xsd:attribute name="siblingRef" type="plm:anyURIType" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute DeltaAddType/@parentRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="parentRef" type="plm:anyURIType" use="optional"/>

attribute DeltaAddType/@siblingRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="siblingRef" type="plm:anyURIType" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy