complexType DeltaDeleteType
diagram plmxml_diagrams/plmxml_p897.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:DeltaOperationBase
properties
base plm:DeltaOperationBase
mixed true
used by
elements DeltaOperationGroupType/Delete PLMXMLDeltaType/Delete
attributes
Name  Type  Use  Default  Fixed  Annotation
targetRefs  plm:uriReferenceListType  required      
annotation
documentation

      This element represents deleting a fragment of PLMXML, i.e. a tree of elements, from
      a master document.
     
      NOTE that it also removes any IDREF or local URI references to those elements, since
      normally you would not want 'dangling' references left. For example, deleting an Instance
      will automatically remove that Instance from any 'instanceRefs' attributes which reference
      it.
     
      Attributes:
     
      targetRefs:       A multiple URI reference to placeholder element(s) which represent the
                        elements in the master document which will be deleted, along with
                        their sub-elements.
     
appinfo
allowMixed=true
source <xsd:complexType name="DeltaDeleteType" mixed="true">
 
<xsd:annotation>
   
<xsd:documentation>
      This element represents deleting a fragment of PLMXML, i.e. a tree of elements, from
      a master document.
     
      NOTE that it also removes any IDREF or local URI references to those elements, since
      normally you would not want 'dangling' references left. For example, deleting an Instance
      will automatically remove that Instance from any 'instanceRefs' attributes which reference
      it.
     
      Attributes:
     
      targetRefs:       A multiple URI reference to placeholder element(s) which represent the
                        elements in the master document which will be deleted, along with
                        their sub-elements.
     
</xsd:documentation>
   
<xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=true</xsd:appinfo>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:DeltaOperationBase">
     
<xsd:attribute name="targetRefs" type="plm:uriReferenceListType" use="required"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute DeltaDeleteType/@targetRefs
type plm:uriReferenceListType
properties
use required
source <xsd:attribute name="targetRefs" type="plm:uriReferenceListType" use="required"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy