complexType DesignRevisionViewType
diagram plmxml_diagrams/plmxml_p287.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:StructureRevisionViewBase
properties
base plm:StructureRevisionViewBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Occurrence plm:PropertyGroup plm:RepresentationEntity plm:EntityPropertyGroup plm:SymbolicOccurrence plm:Representation
used by
element DesignRevisionView
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
revisionRef  plm:anyURIType  optional      
viewRef  plm:anyURIType  optional      
structureViewRef  plm:anyURIType  optional      
instanceRefs  xsd:IDREFS  optional      
gdeInstanceRefs  plm:uriReferenceListType  optional      
connectionInstanceRefs  plm:uriReferenceListType  optional      
signalInstanceRefs  plm:uriReferenceListType  optional      
routeInstanceRefs  plm:uriReferenceListType  optional      
occurrenceRefs  plm:uriReferenceListType  optional      
locationInstanceRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
ruleRefs  plm:uriReferenceListType  optional      
occurrenceControlState  plm:OccurrenceControlEnum    implicit    
representationRefs  xsd:IDREFS  optional      
geometryRefs  plm:uriReferenceListType  optional      
annotation
documentation

      This is a 'view' of a revision of a Design.
     
      Attributes:
     
      representationRefs: Representations of the DesignRevisionView.
      geometryRefs:       geometry elements referenced by the DesignRevisionView.
    
      Elements:

      Representation:     see representationRefs.
     
source <xsd:complexType name="DesignRevisionViewType">
 
<xsd:annotation>
   
<xsd:documentation>
      This is a 'view' of a revision of a Design.
     
      Attributes:
     
      representationRefs: Representations of the DesignRevisionView.
      geometryRefs:       geometry elements referenced by the DesignRevisionView.
    
      Elements:

      Representation:     see representationRefs.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:StructureRevisionViewBase">
     
<xsd:choice minOccurs="0" maxOccurs="unbounded">
       
<xsd:element ref="plm:Representation"/>
     
</xsd:choice>
     
<xsd:attribute name="representationRefs" type="xsd:IDREFS" use="optional" plm:refType="plm:Representation"/>
     
<xsd:attribute name="geometryRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Entity"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute DesignRevisionViewType/@representationRefs
type xsd:IDREFS
properties
use optional
source <xsd:attribute name="representationRefs" type="xsd:IDREFS" use="optional" plm:refType="plm:Representation"/>

attribute DesignRevisionViewType/@geometryRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="geometryRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Entity"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy