complexType ExternalFileType
diagram plmxml_diagrams/plmxml_p316.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:ManagedBase
properties
base plm:ManagedBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound
used by
element ExternalFile
complexType FileType
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
locationRef  plm:anyURIType  required      
format  xsd:string  required      
annotation
documentation

      Represents an external file.

      Attributes:
     
      locationRef: uri of the file
      format:      format of the file. This should determine which applications
                   can read the file. There is no fixed set of values for this, but
                   will often correspond to the file extension, e.g. "doc", "txt".
                   If the format is the same as a Representation format, e.g. "JT",
                   then the same format string should be used.
     
source <xsd:complexType name="ExternalFileType">
 
<xsd:annotation>
   
<xsd:documentation>
      Represents an external file.

      Attributes:
     
      locationRef: uri of the file
      format:      format of the file. This should determine which applications
                   can read the file. There is no fixed set of values for this, but
                   will often correspond to the file extension, e.g. "doc", "txt".
                   If the format is the same as a Representation format, e.g. "JT",
                   then the same format string should be used.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:ManagedBase">
     
<xsd:attribute name="locationRef" type="plm:anyURIType" use="required"/>
     
<xsd:attribute name="format" type="xsd:string" use="required"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute ExternalFileType/@locationRef
type plm:anyURIType
properties
use required
source <xsd:attribute name="locationRef" type="plm:anyURIType" use="required"/>

attribute ExternalFileType/@format
type xsd:string
properties
use required
source <xsd:attribute name="format" type="xsd:string" use="required"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy