complexType ExternalReferenceType
diagram plmxml_diagrams/plmxml_p906.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:AttribOwnerBase
properties
base plm:AttribOwnerBase
children plm:Description plm:ApplicationRef plm:Attribute plm:NGID
used by
element ExternalReference
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
type  xsd:string  optional      
select  xsd:string  optional      
annotation
documentation

      This element is a reference to an object in an Application data model. At present it
      identifies the object by containing one or more ApplicationRef or NGID sub-elements.
     
      Attributes:
     
      type:           Optional PLMXML type of the external object, e.g. "ProductRevision"
     
      select:         If this attribute is present, it will be an XPATH string, which
                      identifies the referenced object relative to a parent object, which
                      is identified by the ApplcationRef sub-elements. The XPATH string will
                      be in terms of the PLMXML schema, but it will be interpreted as
                      applying to the Application data model.
      SubElements:
     
      NGID:           Contains an identifier in NGID format.
     
source <xsd:complexType name="ExternalReferenceType">
 
<xsd:annotation>
   
<xsd:documentation>
      This element is a reference to an object in an Application data model. At present it
      identifies the object by containing one or more ApplicationRef or NGID sub-elements.
     
      Attributes:
     
      type:           Optional PLMXML type of the external object, e.g. "ProductRevision"
     
      select:         If this attribute is present, it will be an XPATH string, which
                      identifies the referenced object relative to a parent object, which
                      is identified by the ApplcationRef sub-elements. The XPATH string will
                      be in terms of the PLMXML schema, but it will be interpreted as
                      applying to the Application data model.
      SubElements:
     
      NGID:           Contains an identifier in NGID format.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:AttribOwnerBase">
     
<xsd:sequence>
       
<xsd:element name="NGID" type="xsd:string" minOccurs="0"/>
     
</xsd:sequence>
     
<xsd:attribute name="type" type="xsd:string" use="optional"/>
     
<xsd:attribute name="select" type="xsd:string" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute ExternalReferenceType/@type
type xsd:string
properties
use optional
source <xsd:attribute name="type" type="xsd:string" use="optional"/>

attribute ExternalReferenceType/@select
type xsd:string
properties
use optional
source <xsd:attribute name="select" type="xsd:string" use="optional"/>

element ExternalReferenceType/NGID
diagram plmxml_diagrams/plmxml_p907.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type xsd:string
properties
minOcc 0
maxOcc 1
content simple
source <xsd:element name="NGID" type="xsd:string" minOccurs="0"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy