complexType GDEBase
diagram plmxml_diagrams/plmxml_p328.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:ManagedBase
properties
base plm:ManagedBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:PropertyGroup
used by
element GDE
complexTypes Ann3DGroupType Annotation3DType ConnectorCavityGroupType ConnectorCavityType ConstraintType FeatureBase LinkBase ProcessorType ProcessVariableType SensorType TerminalType WireCoreType
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
gdeInstanceRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
annotation
documentation

      The GDE element represents an internal constituent of a Structure
      object, such as a Design Feature, Port, Annotation, etc. The Structure
      instances the GDE by means of a GDEInstance.

      Attributes:

      gdeInstanceRefs: a list of references to associated GDEInstances or
                       GDEInstanceGroups. This is to allow the GDE to have
                       internal structure.
      propertyRefs:    reference to properties

      Elements:
     
      PropertyGroup
     
source <xsd:complexType name="GDEBase">
 
<xsd:annotation>
   
<xsd:documentation>
      The GDE element represents an internal constituent of a Structure
      object, such as a Design Feature, Port, Annotation, etc. The Structure
      instances the GDE by means of a GDEInstance.

      Attributes:

      gdeInstanceRefs: a list of references to associated GDEInstances or
                       GDEInstanceGroups. This is to allow the GDE to have
                       internal structure.
      propertyRefs:    reference to properties

      Elements:
     
      PropertyGroup
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:ManagedBase">
     
<xsd:sequence>
       
<xsd:element ref="plm:PropertyGroup" minOccurs="0"/>
     
</xsd:sequence>
     
<xsd:attribute name="gdeInstanceRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Managed"/>
     
<xsd:attribute name="propertyRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Property"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute GDEBase/@gdeInstanceRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="gdeInstanceRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Managed"/>

attribute GDEBase/@propertyRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="propertyRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Property"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy