complexType InitialVelocityType
diagram plmxml_diagrams/plmxml_p864.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:PropertyBase
properties
base plm:PropertyBase
children plm:Description plm:ApplicationRef plm:Attribute
used by
element InitialVelocity
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
ownerRef  plm:anyURIType  optional      
translationVelocity  plm:VectorType  optional      
translationOrientationRef  plm:anyURIType  optional      
rotationVelocity  plm:VectorType  optional      
rotationCentreRef  plm:anyURIType  optional      
annotation
documentation

            The initial translational and rotational velocities of a Mechanism object.

            Attributes:

            translationVelocity: The initial translational velocity of the Mechanism object in SI units,
                            currently metres per second. The default is 0.0, 0.0, 0.0.
            translationOrientationRef: References a Marker, which defines the coordinate system, in which
                            the translational velocity is defined. If the Marker does not hold orientation
                            information, the translational velocity is defined in the coordinate system of
                            the Mechanism object.
            rotationVelocity: The initial rotational velocity of the Mechanism object in SI units,
                            currently radians per second. The default is 0.0, 0.0, 0.0.
            rotationCentreRef: References a Marker, which defines the position of the centre of rotation of
                            the Mechanism object. If the Marker also holds orientation information, the
                            rotational velocity is defined in the coordinate system of the Marker.
                            Otherwise, it is defined in the coordinate system of the Mechanism object. (A
                            Marker may not hold orientation information if it has a translational rather
                            than general Transform sub-element or references a Smart Point rather than a
                            Smart Vector.)
         
source <xsd:complexType name="InitialVelocityType">
 
<xsd:annotation>
   
<xsd:documentation>
            The initial translational and rotational velocities of a Mechanism object.

            Attributes:

            translationVelocity: The initial translational velocity of the Mechanism object in SI units,
                            currently metres per second. The default is 0.0, 0.0, 0.0.
            translationOrientationRef: References a Marker, which defines the coordinate system, in which
                            the translational velocity is defined. If the Marker does not hold orientation
                            information, the translational velocity is defined in the coordinate system of
                            the Mechanism object.
            rotationVelocity: The initial rotational velocity of the Mechanism object in SI units,
                            currently radians per second. The default is 0.0, 0.0, 0.0.
            rotationCentreRef: References a Marker, which defines the position of the centre of rotation of
                            the Mechanism object. If the Marker also holds orientation information, the
                            rotational velocity is defined in the coordinate system of the Marker.
                            Otherwise, it is defined in the coordinate system of the Mechanism object. (A
                            Marker may not hold orientation information if it has a translational rather
                            than general Transform sub-element or references a Smart Point rather than a
                            Smart Vector.)
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:PropertyBase">
     
<xsd:attribute name="translationVelocity" type="plm:VectorType" use="optional"/>
     
<xsd:attribute name="translationOrientationRef" type="plm:anyURIType" use="optional" plm:refType="plm:Marker"/>
     
<xsd:attribute name="rotationVelocity" type="plm:VectorType" use="optional"/>
     
<xsd:attribute name="rotationCentreRef" type="plm:anyURIType" use="optional" plm:refType="plm:Marker"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute InitialVelocityType/@translationVelocity
type plm:VectorType
properties
use optional
facets
Kind Value Annotation
length 3
source <xsd:attribute name="translationVelocity" type="plm:VectorType" use="optional"/>

attribute InitialVelocityType/@translationOrientationRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="translationOrientationRef" type="plm:anyURIType" use="optional" plm:refType="plm:Marker"/>

attribute InitialVelocityType/@rotationVelocity
type plm:VectorType
properties
use optional
facets
Kind Value Annotation
length 3
source <xsd:attribute name="rotationVelocity" type="plm:VectorType" use="optional"/>

attribute InitialVelocityType/@rotationCentreRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="rotationCentreRef" type="plm:anyURIType" use="optional" plm:refType="plm:Marker"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy