complexType JointDataType
diagram plmxml_diagrams/plmxml_p866.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:AttribOwnerBase
properties
base plm:AttribOwnerBase
children plm:Description plm:ApplicationRef plm:Attribute
used by
element JointData
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
type  plm:JointEnum  optional      
annotation
documentation

            Additional data for a Joint Constraint. Only one JointData sub-element is allowed in a
            Constraint, ConstraintInstance or ConstraintOccurrence element.

            Attributes:

            id:             Inherited from AttribOwner.
            name:           Inherited from AttribOwner.
            type:           The type of the Joint as a JointEnum.
         
source <xsd:complexType name="JointDataType">
 
<xsd:annotation>
   
<xsd:documentation>
            Additional data for a Joint Constraint. Only one JointData sub-element is allowed in a
            Constraint, ConstraintInstance or ConstraintOccurrence element.

            Attributes:

            id:             Inherited from AttribOwner.
            name:           Inherited from AttribOwner.
            type:           The type of the Joint as a JointEnum.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:AttribOwnerBase">
     
<xsd:attribute name="type" type="plm:JointEnum" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute JointDataType/@type
type plm:JointEnum
properties
use optional
facets
Kind Value Annotation
enumeration fixed
enumeration atpoint
enumeration inline
enumeration inplane
enumeration orientation
enumeration parallel
enumeration perpendicular
enumeration translational
enumeration revolute
enumeration cylindrical
enumeration universal
enumeration spherical
enumeration planar
enumeration constantVelocity
enumeration screw
source <xsd:attribute name="type" type="plm:JointEnum" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy