complexType JointLimitsType
diagram plmxml_diagrams/plmxml_p867.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:PropertyBase
properties
base plm:PropertyBase
children plm:Description plm:ApplicationRef plm:Attribute plm:RangeWithUnit
used by
element JointLimits
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
ownerRef  plm:anyURIType  optional      
degreeOfFreedom  plm:DegreeOfFreedomEnum  optional      
annotation
documentation

            The linear limits of a translational Joint or the angular limits of a revolute Joint. May
            appear as a sub-element (inside a PropertyGroup) or be referenced by the Joint Constraint.

            Attributes:

            degreeOfFreedom: The degree of freedom of the Joint that the JointLimits limits. Represented as
                            a DegreeOfFreedomEnum.

            Sub-elements:

            RangeWithUnit:  The linear limits of a translational degree of freedom or the angular limits of
                            a rotational degree of freedom. If the units are not specified, SI units are
                            assumed.
         
source <xsd:complexType name="JointLimitsType">
 
<xsd:annotation>
   
<xsd:documentation>
            The linear limits of a translational Joint or the angular limits of a revolute Joint. May
            appear as a sub-element (inside a PropertyGroup) or be referenced by the Joint Constraint.

            Attributes:

            degreeOfFreedom: The degree of freedom of the Joint that the JointLimits limits. Represented as
                            a DegreeOfFreedomEnum.

            Sub-elements:

            RangeWithUnit:  The linear limits of a translational degree of freedom or the angular limits of
                            a rotational degree of freedom. If the units are not specified, SI units are
                            assumed.
         
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:PropertyBase">
     
<xsd:choice minOccurs="1" maxOccurs="1">
       
<xsd:element ref="plm:RangeWithUnit"/>
     
</xsd:choice>
     
<xsd:attribute name="degreeOfFreedom" type="plm:DegreeOfFreedomEnum" use="optional"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute JointLimitsType/@degreeOfFreedom
type plm:DegreeOfFreedomEnum
properties
use optional
facets
Kind Value Annotation
enumeration x
enumeration y
enumeration z
enumeration rx
enumeration ry
enumeration rz
source <xsd:attribute name="degreeOfFreedom" type="plm:DegreeOfFreedomEnum" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy