complexType RepresentationType
diagram plmxml_diagrams/plmxml_p464.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:PropertiesBase
properties
base plm:PropertiesBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:PropertyGroup plm:Transform plm:Parameter plm:InternalRep plm:CompoundRep plm:Material plm:EntityMaterial plm:TextureData plm:Texture plm:EntityTexture plm:EntityRef
used by
elements UGRepType/Representation Representation
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
transformRef  xsd:IDREF  optional      
format  plm:RepresentationFormatType  optional      
revision  xsd:decimal  optional      
location  plm:anyURIType  optional      
appinfo
validate=skipName
load  xsd:boolean    false    
equivalentRef  xsd:IDREF  optional      
type  plm:RepresentationTypeEnum    default    
baseRef  plm:anyURIType  optional      
propertyRefs  plm:uriReferenceListType  optional      
annotation
documentation

      The Representation element in an PLMXML file refers to a model in some
      particular format, such as XT or jXT. It can refer to the model data in
      another file (an External Representation), or the data can be embedded within
      the Representation element in the XML file (an InternalRepresentation). It
      can also consist of a number of CompoundRep sub-elements.

      Attributes:

      format:         data format
      revision:       revision of data
      transformRef:   has the same purpose as the Transform sub-element. Do not use both.
      location:       URI of data source
      load:           true if data is to be loaded at the same time as the PLMXML file.

      equivalentRef:  an optional reference to a Representation which is equivalent to
                      this one (for example, has the same shape). If this attribute is
                      used, then it should collect together equivalent Representations
                      into a ring, with each Representation using this attribute to point
                      to the next in the ring.

      type:           an optional attribute specifying type or purpose of the Representation.
                      Supported values are:
                      "default" - primary or design geometry.
                      "simplified" - geometry of the simplified model.
                      "flat" - geometry of the unfolded model.
                      "user" - the inherited "name" attribute may be set to the name of an NX
                               ReferenceSet, which implies the purpose of the geometry.

                      Representation type can be used to distinguish between additional
                      and alternative geometry at assembly level in the following way:

                      "default"/"user" - If CompoundReps are all of type "construction", "weld"
                               or "midsurface", then geometry should be treated additional.
                               Otherwise - alternative.
                      "simplified" - alternative.
                      "flat" - Not expected at assembly level.

      baseRef:        an optional reference to a Representation which is overridden by this
                      Representation.

      propertyRefs:   A list of references to Properties.

      Elements:

      PropertyGroup:  A collection of Properties.               
      Transform:      optional Transform which positions the geometry in the
                      coordinate frame of the owner.
      Parameter:      Overrides the Parameters on FeatureTree representations.
      CompoundRep:    the Representation may not have a single location. Instead, it may
                      contain a number of CompoundRep sub-elements, each with its own
                      location. The representation is the aggregate of these data sources.
      InternalRep:    the Representation may contain one element derived from InternalRep,
                      in which case it should not also have a location attribute.

      EntityRef:      references to entities in the Representation file. These EntityRef
                      elements can be referenced by RepresentationEntity elements.

      May also contain elements of type Material, EntityMaterial, TextureData, Texture, or
      EntityTexture.
     
source <xsd:complexType name="RepresentationType">
 
<xsd:annotation>
   
<xsd:documentation>
      The Representation element in an PLMXML file refers to a model in some
      particular format, such as XT or jXT. It can refer to the model data in
      another file (an External Representation), or the data can be embedded within
      the Representation element in the XML file (an InternalRepresentation). It
      can also consist of a number of CompoundRep sub-elements.

      Attributes:

      format:         data format
      revision:       revision of data
      transformRef:   has the same purpose as the Transform sub-element. Do not use both.
      location:       URI of data source
      load:           true if data is to be loaded at the same time as the PLMXML file.

      equivalentRef:  an optional reference to a Representation which is equivalent to
                      this one (for example, has the same shape). If this attribute is
                      used, then it should collect together equivalent Representations
                      into a ring, with each Representation using this attribute to point
                      to the next in the ring.

      type:           an optional attribute specifying type or purpose of the Representation.
                      Supported values are:
                      "default" - primary or design geometry.
                      "simplified" - geometry of the simplified model.
                      "flat" - geometry of the unfolded model.
                      "user" - the inherited "name" attribute may be set to the name of an NX
                               ReferenceSet, which implies the purpose of the geometry.

                      Representation type can be used to distinguish between additional
                      and alternative geometry at assembly level in the following way:

                      "default"/"user" - If CompoundReps are all of type "construction", "weld"
                               or "midsurface", then geometry should be treated additional.
                               Otherwise - alternative.
                      "simplified" - alternative.
                      "flat" - Not expected at assembly level.

      baseRef:        an optional reference to a Representation which is overridden by this
                      Representation.

      propertyRefs:   A list of references to Properties.

      Elements:

      PropertyGroup:  A collection of Properties.               
      Transform:      optional Transform which positions the geometry in the
                      coordinate frame of the owner.
      Parameter:      Overrides the Parameters on FeatureTree representations.
      CompoundRep:    the Representation may not have a single location. Instead, it may
                      contain a number of CompoundRep sub-elements, each with its own
                      location. The representation is the aggregate of these data sources.
      InternalRep:    the Representation may contain one element derived from InternalRep,
                      in which case it should not also have a location attribute.

      EntityRef:      references to entities in the Representation file. These EntityRef
                      elements can be referenced by RepresentationEntity elements.

      May also contain elements of type Material, EntityMaterial, TextureData, Texture, or
      EntityTexture.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:PropertiesBase">
     
<xsd:sequence>
       
<xsd:element ref="plm:PropertyGroup" minOccurs="0"/>
       
<xsd:element ref="plm:Transform" minOccurs="0"/>
       
<xsd:element name="Parameter" type="plm:UserDataElementType" minOccurs="0" maxOccurs="unbounded"/>
       
<xsd:element ref="plm:InternalRep" minOccurs="0"/>
       
<xsd:element ref="plm:CompoundRep" minOccurs="0" maxOccurs="unbounded"/>
       
<xsd:choice minOccurs="0" maxOccurs="unbounded">
         
<xsd:element ref="plm:Material"/>
         
<xsd:element ref="plm:EntityMaterial"/>
         
<xsd:element ref="plm:TextureData"/>
         
<xsd:element ref="plm:Texture"/>
         
<xsd:element ref="plm:EntityTexture"/>
         
<xsd:element ref="plm:EntityRef"/>
       
</xsd:choice>
     
</xsd:sequence>
     
<xsd:attribute name="transformRef" type="xsd:IDREF" use="optional" plm:refType="plm:Transform"/>
     
<xsd:attribute name="format" type="plm:RepresentationFormatType" use="optional"/>
     
<xsd:attribute name="revision" type="xsd:decimal" use="optional"/>
     
<xsd:attributeGroup ref="plm:referenceGroup"/>
     
<xsd:attribute name="equivalentRef" type="xsd:IDREF" use="optional" plm:refType="plm:Representation"/>
     
<xsd:attribute name="type" type="plm:RepresentationTypeEnum" default="default"/>
     
<xsd:attribute name="baseRef" type="plm:anyURIType" use="optional"/>
     
<xsd:attribute name="propertyRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Property"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute RepresentationType/@transformRef
type xsd:IDREF
properties
use optional
source <xsd:attribute name="transformRef" type="xsd:IDREF" use="optional" plm:refType="plm:Transform"/>

attribute RepresentationType/@format
type plm:RepresentationFormatType
properties
use optional
facets
Kind Value Annotation
enumeration XT
enumeration eXT
enumeration PLMXML
enumeration jXT
enumeration JT
enumeration XPK
enumeration XGL
enumeration VRML
enumeration STL
enumeration SAT
enumeration STEP
enumeration IGES
enumeration UGBkm
enumeration UGPrt
enumeration SEPrt
enumeration SEAsm
enumeration IdeasPrt
enumeration IdeasAsm
enumeration IdeasIDI
enumeration Cat4Prt
enumeration Cat5Prt
enumeration Cat5Asm
enumeration SWPrt
enumeration SWAsm
enumeration IDI
enumeration TX
enumeration DWG
enumeration DWF
enumeration DXF
enumeration ProE
enumeration CGM
enumeration CGR
enumeration Unregistered
source <xsd:attribute name="format" type="plm:RepresentationFormatType" use="optional"/>

attribute RepresentationType/@revision
type xsd:decimal
properties
use optional
source <xsd:attribute name="revision" type="xsd:decimal" use="optional"/>

attribute RepresentationType/@equivalentRef
type xsd:IDREF
properties
use optional
source <xsd:attribute name="equivalentRef" type="xsd:IDREF" use="optional" plm:refType="plm:Representation"/>

attribute RepresentationType/@type
type plm:RepresentationTypeEnum
properties
default default
facets
Kind Value Annotation
enumeration default
enumeration simplified
enumeration flat
enumeration user
source <xsd:attribute name="type" type="plm:RepresentationTypeEnum" default="default"/>

attribute RepresentationType/@baseRef
type plm:anyURIType
properties
use optional
source <xsd:attribute name="baseRef" type="plm:anyURIType" use="optional"/>

attribute RepresentationType/@propertyRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="propertyRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Property"/>

element RepresentationType/Parameter
diagram plmxml_diagrams/plmxml_p465.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type plm:UserDataElementType
properties
minOcc 0
maxOcc unbounded
content complex
children plm:UserList
attributes
Name  Type  Use  Default  Fixed  Annotation
title  xsd:string  required      
value  xsd:string  required      
type  plm:UserValueDataType    string    
format  xsd:string  optional      
dataRef  plm:anyURIType  optional      
editable  xsd:boolean    false    
minInclusive  xsd:double  optional      
minExclusive  xsd:double  optional      
maxInclusive  xsd:double  optional      
maxExclusive  xsd:double  optional      
stepValue  xsd:double  optional      
minLength  xsd:nonNegativeInteger  optional      
maxLength  xsd:nonNegativeInteger  optional      
titleRef  plm:anyURIType  optional      
valueRef  plm:anyURIType  optional      
source <xsd:element name="Parameter" type="plm:UserDataElementType" minOccurs="0" maxOccurs="unbounded"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy