complexType UnitComponentType
diagram plmxml_diagrams/plmxml_p529.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
used by
elements UnitType/Ampere UnitType/Candela UnitType/Kelvin UnitType/Kilogram UnitType/Metre UnitType/Mole UnitType/Second
attributes
Name  Type  Use  Default  Fixed  Annotation
exponent  xsd:double    1    
prefix  plm:UnitPrefixType  optional      
annotation
documentation

      Component of a standard SI unit of measurement

      Attributes:
     
      prefix:      multiplier prefix, e.g. "kilo", "micro"
      exponent:    power to which unit is raised, e.g. seconds**-2
     
source <xsd:complexType name="UnitComponentType">
 
<xsd:annotation>
   
<xsd:documentation>
      Component of a standard SI unit of measurement

      Attributes:
     
      prefix:      multiplier prefix, e.g. "kilo", "micro"
      exponent:    power to which unit is raised, e.g. seconds**-2
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:attribute name="exponent" type="xsd:double" default="1"/>
 
<xsd:attribute name="prefix" type="plm:UnitPrefixType" use="optional"/>
</xsd:complexType>

attribute UnitComponentType/@exponent
type xsd:double
properties
default 1
source <xsd:attribute name="exponent" type="xsd:double" default="1"/>

attribute UnitComponentType/@prefix
type plm:UnitPrefixType
properties
use optional
facets
Kind Value Annotation
enumeration yotta
enumeration zetta
enumeration exa
enumeration peta
enumeration tera
enumeration giga
enumeration mega
enumeration kilo
enumeration hecto
enumeration deka
enumeration deci
enumeration centi
enumeration milli
enumeration micro
enumeration nano
enumeration pico
enumeration femto
enumeration atto
enumeration zepto
enumeration yocto
source <xsd:attribute name="prefix" type="plm:UnitPrefixType" use="optional"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy