complexType ValidationRequirementRevisionType
diagram plmxml_diagrams/plmxml_p1425.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:DesignRequirementRevisionType
properties
base plm:DesignRequirementRevisionType
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:VariantDefault plm:VariantRuleCheck plm:PropertyGroup plm:PlainText plm:Message
used by
element ValidationRequirementRevision
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
revision  xsd:string  required      
version  xsd:nonNegativeInteger  optional      
masterRef  plm:anyURIType  required      
optionRefs  plm:uriReferenceListType  optional      
instanceRefs  plm:uriReferenceListType  optional      
gdeInstanceRefs  plm:uriReferenceListType  optional      
simplifiedRepRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
plainRef  plm:anyURIType  optional      
parameterRefs  plm:uriReferenceListType        
expressionRef  plm:anyURIType        
annotation
documentation

      A revision of a requirement for validation.
     
      Attributes:
     
      expressionRef:    References the ValidationExpression for the requirement.
     
      Sub-elements:
     
      Message:          The status of the validation. An InformMessage indicates
                        pass. An ErrorMessage indicates failure. A WarnMessage
                        indicates a warning. A CheckMessage indicates no
                        specific semantics.
     
source <xsd:complexType name="ValidationRequirementRevisionType">
 
<xsd:annotation>
   
<xsd:documentation>
      A revision of a requirement for validation.
     
      Attributes:
     
      expressionRef:    References the ValidationExpression for the requirement.
     
      Sub-elements:
     
      Message:          The status of the validation. An InformMessage indicates
                        pass. An ErrorMessage indicates failure. A WarnMessage
                        indicates a warning. A CheckMessage indicates no
                        specific semantics.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:DesignRequirementRevisionType">
     
<xsd:choice minOccurs="0">
       
<xsd:element ref="plm:Message"/>
     
</xsd:choice>
     
<xsd:attribute name="expressionRef" type="plm:anyURIType" plm:refType="plm:ValidationExpression"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute ValidationRequirementRevisionType/@expressionRef
type plm:anyURIType
source <xsd:attribute name="expressionRef" type="plm:anyURIType" plm:refType="plm:ValidationExpression"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy