complexType WorkAreaOccurrenceType
diagram plmxml_diagrams/plmxml_p1085.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:OccurrenceType
properties
base plm:OccurrenceType
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:Transform plm:Representation plm:VariantCondition plm:Reference plm:PropertyGroup plm:EntityPropertyGroup plm:Material plm:EntityMaterial plm:AssociatedAttachment plm:AttributeContext
used by
element WorkAreaOccurrence
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
instancedRef  plm:anyURIType  optional      
transformRef  xsd:IDREF  optional      
materialRef  xsd:IDREF  optional      
partRef  plm:anyURIType  optional      
representationRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
designRequired  xsd:boolean  optional      
occurrenceRefs  xsd:IDREFS  optional      
instanceRefs  plm:uriReferenceListType  optional      
pathRefs  plm:uriReferenceListType  optional      
geometryRefs  plm:uriReferenceListType  optional      
alternativeOfRef  plm:anyURIType  optional      
productViewRef  plm:anyURIType  optional      
visible  xsd:boolean  optional      
lastInstanceParentRef  plm:anyURIType  optional      
sourceRef  plm:anyURIType  optional      
linkedOccurrenceRef  plm:anyURIType  optional      
linkedGroupRef  plm:anyURIType  optional      
associatedAttachmentRefs  plm:uriReferenceListType  optional      
parentRef  plm:anyURIType  optional      
instanceNumber  xsd:integer  optional      
occurrenceId  xsd:string  optional      
controlRefs  plm:uriReferenceListType  optional      
symbolicRefs  plm:uriReferenceListType  optional      
predecessorRefs  plm:uriReferenceListType  optional      
annotation
documentation

      This is a derived class of Occurrence, specific to WorkArea Structure.
     
      Attributes:
     
      predecessorRefs:            list of predecessor WorkAreaOccurrences
     
source <xsd:complexType name="WorkAreaOccurrenceType">
 
<xsd:annotation>
   
<xsd:documentation>
      This is a derived class of Occurrence, specific to WorkArea Structure.
     
      Attributes:
     
      predecessorRefs:            list of predecessor WorkAreaOccurrences
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:OccurrenceType">
     
<xsd:attribute name="predecessorRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:WorkAreaOccurrence"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute WorkAreaOccurrenceType/@predecessorRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="predecessorRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:WorkAreaOccurrence"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy