| diagram | ![]() |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| type | extension of plm:ManagedBase | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| children | plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| used by |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| attributes |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| annotation |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:complexType name="InstancePathType"> <xsd:annotation> <xsd:documentation> This element represents an unconfigured path of InstanceThreads, top to bottom. The path must be sequential in that the 'instanced' Structure of each InstanceThread must be the same as the 'parent' Structure of the next InstanceThread in the path. It is possible (although unusual) for an InstancePath to 'change views' as you go down the path. Attributes: instancePathRootRef: The InstancePathRoot which represents the top of the tree this InstancePath is in. instanceThreadRef: This is the last (bottom) InstanceThread in the instance path. (Unlike the Occurrence element, which has an "instanceRefs" attribute to specify the full path, this element only specifies the last InstanceThread, and relies on its 'ancestor' elements to define the path). childRefs: the 'children' of the InstancePath. This is a selection of other InstancePaths, each of which must have a path which is formed by adding one more InstanceThread on the end of the path. There must be no duplicates paths. absoluteOccurrenceRef: This is a back-pointer to a referencing AbsoluteOccurrence (There can be at most one AbsoluteOccurrence referencing a given InstancePath) </xsd:documentation> </xsd:annotation> <xsd:complexContent> <xsd:extension base="plm:ManagedBase"> <xsd:attribute name="instancePathRootRef" type="plm:anyURIType" use="optional" plm:refType="plm:InstancePathRoot"/> <xsd:attribute name="instanceThreadRef" type="plm:anyURIType" use="optional" plm:refType="plm:InstanceThread"/> <xsd:attribute name="childRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:InstancePath"/> <xsd:attribute name="absoluteOccurrenceRef" type="plm:anyURIType" plm:refType="plm:AbsoluteOccurrence"/> </xsd:extension> </xsd:complexContent> </xsd:complexType> |
| type | plm:anyURIType | ||
| properties |
|
||
| source | <xsd:attribute name="instancePathRootRef" type="plm:anyURIType" use="optional" plm:refType="plm:InstancePathRoot"/> |
| type | plm:anyURIType | ||
| properties |
|
||
| source | <xsd:attribute name="instanceThreadRef" type="plm:anyURIType" use="optional" plm:refType="plm:InstanceThread"/> |
| type | plm:uriReferenceListType | ||
| properties |
|
||
| source | <xsd:attribute name="childRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:InstancePath"/> |
| type | plm:anyURIType |
| source | <xsd:attribute name="absoluteOccurrenceRef" type="plm:anyURIType" plm:refType="plm:AbsoluteOccurrence"/> |