| diagram | ![]() |
||||||||||||||||||||||||||||||||||||||||||||||||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||||||||||||||||||||||||||
| type | extension of plm:AttribOwnerBase | ||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
||||||||||||||||||||||||||||||||||||||||||||||||
| children | plm:Description plm:ApplicationRef plm:Attribute plm:Transform | ||||||||||||||||||||||||||||||||||||||||||||||||
| used by |
|
||||||||||||||||||||||||||||||||||||||||||||||||
| attributes |
|
||||||||||||||||||||||||||||||||||||||||||||||||
| annotation |
|
||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:complexType name="MotionEntityRefType"> <xsd:annotation> <xsd:documentation> Applies a Transform sub-element to one or more conceptual motion entities or bodies. A MotionEntityRef may have an absolute or relative Transform. Attributes: transformType: Specifies whether the Transform sub-element is applied to the MotionEntity elements referenced by the motionEntityRefs attribute absolutely or relatively (the default). An absolute MotionEntityRef applies its Transform to the MotionEntity elements in the absolute coordinate system. A relative MotionEntityRef applies its Transform relative to the positions and orientations of the MotionEntity elements in a previous Frame. Those positions and orientations are usually defined by the Transform sub-element of a MotionEntityRef in a previous Frame. However, if no previous Frame has a MotionEntityRef that applies to the MotionEntity elements and that has a Transform sub-element, the positions and orientations are defined by the playback application. motionEntityRefs: References MotionEntity elements, which represent the conceptual motion entities or bodies. Sub-elements: Transform: The Transform that is applied to the MotionEntity elements referenced by the motionEntityRefs attribute. </xsd:documentation> </xsd:annotation> <xsd:complexContent> <xsd:extension base="plm:AttribOwnerBase"> <xsd:choice minOccurs="0" maxOccurs="1"> <xsd:element ref="plm:Transform"/> </xsd:choice> <xsd:attribute name="transformType" type="plm:MotionTransformEnum" default="relative"/> <xsd:attribute name="motionEntityRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:MotionEntity"/> </xsd:extension> </xsd:complexContent> </xsd:complexType> |
| type | plm:MotionTransformEnum | |||||||||
| properties |
|
|||||||||
| facets |
|
|||||||||
| source | <xsd:attribute name="transformType" type="plm:MotionTransformEnum" default="relative"/> |
| type | plm:uriReferenceListType | ||
| properties |
|
||
| source | <xsd:attribute name="motionEntityRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:MotionEntity"/> |