| diagram | ![]() |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| type | extension of plm:AttribOwnerBase | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| children | plm:Description plm:ApplicationRef plm:Attribute plm:StiffnessExpression | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| used by |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| attributes |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| annotation |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:complexType name="SpringDataType"> <xsd:annotation> <xsd:documentation> Additional data for a Spring Constraint. Only one SpringData sub-element is allowed in a Constraint, ConstraintInstance or ConstraintOccurrence element. Attributes: id: Inherited from AttribOwner. name: Inherited from AttribOwner. degreeOfFreedom: The degree of freedom of the Joint along or around which the Spring acts. Represented as a DegreeOfFreedomEnum. preloadForce: The preload force or torque in SI units, currently newtons for forces acting along translational degrees of freedom and newton metres for torques acting around rotational degrees of freedom. The default is 0.0. stiffness: The spring constant of a Spring in SI units, currently newtons per metre for Springs acting along translational degrees of freedom and newton metres per radian for Springs acting around rotational degrees of freedom. The default is 0.0. This is ignored when there is a StiffnessExpression sub-element. free: The free length or angle of a Spring in SI units, currently metres for Springs acting along translational degrees of freedom and radians for Springs acting around rotational degrees of freedom. The default is 0.0. Sub-element: StiffnessExpression: A MechanismExpression that defines the spring constant of a non-linear Spring in SI units. (newtons per metre along translational degrees of freedom and newton metres per radian around rotational degrees of freedom.) </xsd:documentation> </xsd:annotation> <xsd:complexContent> <xsd:extension base="plm:AttribOwnerBase"> <xsd:choice minOccurs="0"> <xsd:element name="StiffnessExpression" type="plm:MechanismExpressionType"/> </xsd:choice> <xsd:attribute name="degreeOfFreedom" type="plm:DegreeOfFreedomEnum" use="optional"/> <xsd:attribute name="preloadForce" type="xsd:double" default="0.0"/> <xsd:attribute name="stiffness" type="xsd:double" default="0.0"/> <xsd:attribute name="free" type="xsd:double" default="0.0"/> </xsd:extension> </xsd:complexContent> </xsd:complexType> |
| type | plm:DegreeOfFreedomEnum | |||||||||||||||||||||
| properties |
|
|||||||||||||||||||||
| facets |
|
|||||||||||||||||||||
| source | <xsd:attribute name="degreeOfFreedom" type="plm:DegreeOfFreedomEnum" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="preloadForce" type="xsd:double" default="0.0"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="stiffness" type="xsd:double" default="0.0"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="free" type="xsd:double" default="0.0"/> |
| diagram | ![]() |
||||||||||||||||||||||||||||||||||||||||||||||||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||||||||||||||||||||||||||
| type | plm:MechanismExpressionType | ||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
||||||||||||||||||||||||||||||||||||||||||||||||
| children | plm:Description plm:ApplicationRef plm:Attribute | ||||||||||||||||||||||||||||||||||||||||||||||||
| attributes |
|
||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:element name="StiffnessExpression" type="plm:MechanismExpressionType"/> |