| diagram | ![]() |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| namespace | http://www.plmxml.org/Schemas/PLMXMLSchema | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| type | extension of plm:AttribOwnerBase | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| properties |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| children | plm:Description plm:ApplicationRef plm:Attribute | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| used by |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| attributes |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| annotation |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| source | <xsd:complexType name="ThreadType"> <xsd:annotation> <xsd:documentation> This element describes a Thread. Note: the thread defaults to right-handed. An attribute to indicate left-handed may be added in the future if required. Attributes: type: The type (standard) of thread. Some possible values are: ANSI threads: UNC, UNF, UNEF ANSI pipe threads: NPSM, NPT ISO threads: M ISO pipe threads: Rp, Rc This attribute is a string to allow custom standards. extent: The extent type of the thread. length: The length of the thread, if extent = 'finite'. offset: The offset distance, from the start of the owning feature, before the thread starts. nominalDiameter: Nominal diameter, i.e. diameter of cylinder to which the thread applies. internalDiameter: Diameter as applied to inside of thread. externalDiameter: Diameter as applies to outside of thread. For these three diameters we have: internalDiameter .LT. nominalDiameter .LT. externalDiameter designateDiameter: Designated diameter. This is a string, e.g. "M8". effectiveLength: This is the length of the thread which is cut at full depth. height: The distance from the inside of the thread to the outside of the thread. taperAngle: The angle of taper, in radians. This is positive and less than pi/2. The taper is always towards the centreline, in the direction of the thread. pitch: The distance between adjacent threads, measured along the length of the thread, in metres (SI units). </xsd:documentation> </xsd:annotation> <xsd:complexContent> <xsd:extension base="plm:AttribOwnerBase"> <xsd:attribute name="type" type="xsd:string" use="optional"/> <xsd:attribute name="extent" type="plm:ThreadExtentType" use="optional"/> <xsd:attribute name="length" type="xsd:double" use="optional"/> <xsd:attribute name="offset" type="xsd:double" use="optional"/> <xsd:attribute name="nominalDiameter" type="xsd:double" use="optional"/> <xsd:attribute name="internalDiameter" type="xsd:double" use="optional"/> <xsd:attribute name="externalDiameter" type="xsd:double" use="optional"/> <xsd:attribute name="designateDiameter" type="xsd:string" use="optional"/> <xsd:attribute name="effectiveLength" type="xsd:double" use="optional"/> <xsd:attribute name="height" type="xsd:double" use="optional"/> <xsd:attribute name="taperAngle" type="xsd:double" use="optional"/> <xsd:attribute name="pitch" type="xsd:double" use="optional"/> </xsd:extension> </xsd:complexContent> </xsd:complexType> |
| type | xsd:string | ||
| properties |
|
||
| source | <xsd:attribute name="type" type="xsd:string" use="optional"/> |
| type | plm:ThreadExtentType | |||||||||
| properties |
|
|||||||||
| facets |
|
|||||||||
| source | <xsd:attribute name="extent" type="plm:ThreadExtentType" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="length" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="offset" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="nominalDiameter" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="internalDiameter" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="externalDiameter" type="xsd:double" use="optional"/> |
| type | xsd:string | ||
| properties |
|
||
| source | <xsd:attribute name="designateDiameter" type="xsd:string" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="effectiveLength" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="height" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="taperAngle" type="xsd:double" use="optional"/> |
| type | xsd:double | ||
| properties |
|
||
| source | <xsd:attribute name="pitch" type="xsd:double" use="optional"/> |