complexType GDEInstanceGroupType
diagram plmxml_diagrams/plmxml_p329.png
namespace http://www.plmxml.org/Schemas/PLMXMLSchema
type extension of plm:ManagedBase
properties
base plm:ManagedBase
children plm:Description plm:ApplicationRef plm:Attribute plm:BoxBound plm:SphereBound plm:Bound plm:GDEInstance plm:PropertyGroup
used by
element GDEInstanceGroup
complexType Ann3DInstanceGroupType
attributes
Name  Type  Use  Default  Fixed  Annotation
id  xsd:ID  optional      
name  xsd:string  optional      
nameRef  plm:anyURIType  optional      
descriptionTextRef  plm:anyURIType  optional      
attributeRefs  xsd:IDREFS  optional      
accessRefs  plm:uriReferenceListType  optional      
statusRef  plm:anyURIType  optional      
checkoutRefs  plm:uriReferenceListType  optional      
subType  xsd:string  optional      
effectivityRefs  plm:uriReferenceListType  optional      
releaseStatusRefs  plm:uriReferenceListType  optional      
propertyRefs  plm:uriReferenceListType  optional      
annotation
documentation

      GDEInstanceGroup: derived from Managed.

      This global element is used to collect together a number of
      GDEInstance elements to simplify referencing.

      Attributes:

      propertyRefs     Reference to Properties.

      Elements:
     
      GDEInstance      Any number of GDEInstances.
      PropertyGroup    A group of Properties applicable to all GDEInstances
                       in the GDEInstanceGroup.
     
source <xsd:complexType name="GDEInstanceGroupType">
 
<xsd:annotation>
   
<xsd:documentation>
      GDEInstanceGroup: derived from Managed.

      This global element is used to collect together a number of
      GDEInstance elements to simplify referencing.

      Attributes:

      propertyRefs     Reference to Properties.

      Elements:
     
      GDEInstance      Any number of GDEInstances.
      PropertyGroup    A group of Properties applicable to all GDEInstances
                       in the GDEInstanceGroup.
     
</xsd:documentation>
 
</xsd:annotation>
 
<xsd:complexContent>
   
<xsd:extension base="plm:ManagedBase">
     
<xsd:sequence>
       
<xsd:element ref="plm:GDEInstance" minOccurs="0" maxOccurs="unbounded"/>
       
<xsd:element ref="plm:PropertyGroup" minOccurs="0"/>
     
</xsd:sequence>
     
<xsd:attribute name="propertyRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Property"/>
   
</xsd:extension>
 
</xsd:complexContent>
</xsd:complexType>

attribute GDEInstanceGroupType/@propertyRefs
type plm:uriReferenceListType
properties
use optional
source <xsd:attribute name="propertyRefs" type="plm:uriReferenceListType" use="optional" plm:refType="plm:Property"/>


XML Schema documentation generated by XMLSpy Schema Editor http://www.altova.com/xmlspy